[MPC8640D]:Unable to initialize sRIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC8640D]:Unable to initialize sRIO

1,945 Views
Arathi
Contributor II

Hi NXP Support Team,

We are having a custom board with MPC8640D PowerPC architecture processor.
A sRIO switch is connected to this processor.

While loading our custom Linux image we are unable to initialize the sRIO and we are getting segmentation fault. 

Attaching the log file for your reference.
Please find the highlighted sRIO init failing part

Please help me resolve this issue

Regards,
Arathi

 

0 Kudos
Reply
1 Reply

1,905 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

Line 171: fsl-of-rio e00c0000.rapidio: Of-device full name /rapidio@e00c0000
Line 172: fsl-of-rio e00c0000.rapidio: Regs: [mem 0xe00c0000-0xe00dffff]
Line 173: fsl-of-rio e00c0000.rapidio: bellirq: 50
Line 174: fsl-of-rio e00c0000.rapidio: pwirq: 48
Line 175: fsl-of-rio e00c0000.rapidio: /rapidio@e00c0000/port1: LAW start 0x00000000c0000000, size 0x0000000020000000.
Line 177: fsl-of-rio e00c0000.rapidio: RapidIO PHY type: Serial
Line 178: fsl-of-rio e00c0000.rapidio: Port 0 is not ready. Try to restart connection...
Line 179: fsl-of-rio e00c0000.rapidio: Port 0 restart failed.
Line 180: fsl-of-rio: probe of e00c0000.rapidio failed with error -67

In the boot log, there are errors reported. Due to we haven't the board and software to reproduce, I suggest customer to add some debug message in rapidio driver, check the failed errors first.

0 Kudos
Reply