MPC8610 - Kernel Upgrade

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8610 - Kernel Upgrade

1,072 Views
glabarthe
Contributor I

Hi everyone,

I am currently trying to upgrade my freescale MPC8610 linux kernel from 2.6.23 to 2.6.31 in order to be able to use the performance counters.

However, I am facing some difficulties.

Here is what I did :

  • I built my new kernel using the mpc8610_hpcd default configuration and performance counters enabled.
  • Then i have generated the dtb file corresponding to my board.
  • Finally i use u-boot (version 1.3) to load the dtb and the uImage and boot the kernel.

When I boot, u-boot stops after loading the dtb file.

I suspect that my u-boot version is too old, but I'm not sure if I can safely upgrade it ?

I googled a lot about the subject but didn't find anything helpful.

Did anyone do that kind of upgrade (kernel and/or u-boot) ?

Thank you.

Best regards.

Guillaume LABARTHE.

0 Kudos
Reply
0 Replies