MPC8360 boot after HRESET

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8360 boot after HRESET

2,786 次查看
Willow
Contributor I
We have a problem with HRESET.
 
The system load the config words RCWHR (xB4600002) and RCWLR (x04030005) onto the local bus after POReset,  This works fine and we have no problems with it.
 
However if we assert HRESET (from the watchdog) it goes through the same sequence but does not boot.
 
SRESET is also fine.
 
any ideas.
 
Regards
 
Willow
0 项奖励
回复
3 回复数

1,888 次查看
hw_engineer
Contributor I
I don´t know your exact reset sequence so i can guess only.

POReset: processor and everthing else powers up --> enough start up time for flash
HReset: 16 clock cycles are to short to reset your flash and to be ready to serve RCW
SReset: no problem cause no flash reset is caused?!

these are only some ideas...
0 项奖励
回复

1,888 次查看
hw_engineer
Contributor I
We also have a problem with booting from local bus. The Core is freezed after loading the config words.

Are you sure that your flash is properly out of reset and all timings are fulfilled? Some flash need up to 35µs to come out of reset...
0 项奖励
回复

1,888 次查看
Willow
Contributor I
Would the Flash Timing be any different to the reponse after POReset? 
 
We have no problem with POReset or SReset,  just HReset.
 
 
0 项奖励
回复