MPC8308CVMAGDA EXCEPTION 0055255

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8308CVMAGDA EXCEPTION 0055255

1,468 Views
ShaneMaynard
Contributor I

Does anyone have an explanation for the exception on the part number above. We require MPC8308CVMAGDA, however the parts received are marked with SPC8308CVMAFDA, AF part number ending indicates 333Mhz but the required part number denotes 400Mhz. The device also has an addition 'M' marking in the top right corner which i haven't see previously, has this been added as part of the exception? Will the part have the same functionality? 

I have attached a photo of the device and the label received. 

2 Replies

1,412 Views
NEEDEOLCALL
Contributor III

You can ask the supplier if they have COC certificate. Only the supplier with COC certificate is the real original supplier.

0 Kudos
Reply

1,412 Views
NEEDEOLCALL
Contributor III

You bought a fake product. Return it immediately.
This is a scam.
I can send you the correct images. Our PCB factory takes photos.1.png

0 Kudos
Reply