MPC567xKEVB including P&E Micro debugger.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC567xKEVB including P&E Micro debugger.

1,693件の閲覧回数
iggi
NXP Employee
NXP Employee

This message is posted to make the information available on the web, since there wasn't any data about the feature of the EVB kit.

 

MPC5675KEVB257/473 Evaluation Kit comes with P&E's USB QORIVVA MPC55xx/56xx MULTILINK (the blue one).

 

Use the links below as a reference.

 

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320021

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC567xKEVB


タグ(2)
0 件の賞賛
返信
1 返信

1,364件の閲覧回数
jonr
Contributor III

Thanks.  If somone wants to loan me one, I will make O5E (open5xxxecu.org) run on it.

0 件の賞賛
返信