MMPF0100F6ANES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100F6ANES

1,388件の閲覧回数
RamakrishnaC
Contributor III

Hi Team,

Regarding PWRON, STANDBY & SDWNB pins, We are not using any battery and power ON switch botton. Still these pins need to connect to i.Mx6Q processor?

If we need to connect what is the use of PWRON, STANDBY & SDWNB pins?

Please explain clarly on this pins use without battery and switch.

FYI, In my design we are using i.Mx6Q. &  MMPF0100F6ANES Pre-programmed OTP configuration F6.

RamakrishnaC_0-1726042956742.png

Thank you.

 

0 件の賞賛
返信
3 返答(返信)

1,373件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Ramakrishna,

please refer to the Table 1. in the AN4717. There is recommended connection for some pins when they are not used. 

The PWRON pin is an input. It must be connected. If you don't need to use it's funtion, please connect it to VSNVS pin via an 8k to 100k pull-up resistor. A middle pull-up resistor should be ok. E.g. 50kOhm. 

JozefKozon_0-1726052178530.png

You can leave the RESETBMCU floating. 

JozefKozon_1-1726052243595.png

Connect the unused STANDBY pin to ground.

JozefKozon_2-1726052300566.png

Please leave the unused SDWNB floating.

JozefKozon_3-1726052383710.png

With Best Regards,

Jozef

 

0 件の賞賛
返信

1,370件の閲覧回数
RamakrishnaC
Contributor III

Hi JozefKozon, 

Thank you.

Here I have another doubt without coin cell and switch. Is there any use of these pins?

-STANDBY

-SDWNB

-PWRON

Please confirm we are using i.Mx6Q and PMIC. with this combination. we want to understand more about these pin functionality without coin cell and switch.

Thank you.

 

0 件の賞賛
返信

1,353件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Ramakrishna,

PWRON, STANDBY & SDWNB

the three pins above have nothing to do with the LICELL pin. If you don't need to use the Coin Cell, you will have no backup power, when the VIN power is not available. Depends on your requirements.

The PWRON pin can be used to restart the PMIC by your MCU (i.MX6Q). 

JozefKozon_0-1726053925212.png

The STANBY pin can send the PMIC to Standby mode. It can be again driven by the MCU.

JozefKozon_2-1726054084465.png

If you will not use the STANBY pin, then you don't need the coin cell 3V backup. Connecting the STANBY pin to Ground as recommended when not used will keep the STANBY pin constantly at 0V.  

The SDWNB pin is an output from the PMIC. If you will not use it, your MCU will not be notified. 

JozefKozon_1-1726053976743.png

The above pins are not mandatory to use if you don't need their functions. It's up to you if you need the functions or not. If not used, please follow the AN4717 for recommended connections when unused.

With Best Regards,

Jozef

 

 

0 件の賞賛
返信