MMPF0100F6ANES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100F6ANES

6,468件の閲覧回数
RamakrishnaC
Contributor III

HI Team,

MMPF0100F6ANES, In this part i am not using the VIN1, VIN2, SW2 and SW4. as per NXP reference document  need connect >3.4V to VIN1 & VIN2 without using the outputs. So shall i connect VGEN6 output(3V) to VIN1 & VIN2?

Please confirm.

Thanks.

0 件の賞賛
返信
5 返答(返信)

6,425件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello RamakrishnaC,

I hope all is great with you. Thank you for using the NXP communities.

Correct. Based on the document attached, if VIN1 and VIN2 are not used, they must be connected to the output of a regulator with voltage <3.4V and <3.6V respectively.

I hope this information helps.

Regards,

David

0 件の賞賛
返信

6,409件の閲覧回数
RamakrishnaC
Contributor III

Hi David,

Thank you.

My queation is shall i connecet the other voltage regulator output to VIN1 & VIN2?

Please review and check my scheamtic complete PMIC configuration and share your feedback details.

Thank you.

0 件の賞賛
返信

6,395件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello RamakrishnaC,

Once again, thank you for using the NXP community.

Correct, as long as the output of a regulator is <3.4V and <3.6V respectively.

diazmarin09_0-1719504371438.png

 

Your schematic seems correct to me.

Regards,

David

0 件の賞賛
返信

6,393件の閲覧回数
RamakrishnaC
Contributor III

Hi David,

Thank you.

And one more conformation needed. 

Can i connect the VGEN6 output voltage to VIN1 & VIN2?

Please confirm.

0 件の賞賛
返信

6,390件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello RamakrishnaC,

Yes, you can. As long as VIN3 is supplied, you can connect the VGEN6 output to VIN1 and VIN2.

diazmarin09_0-1719512885576.png

 

I hope this information helps.

Regards,

David

0 件の賞賛
返信