MMA6827

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA6827

1,791 Views
Zhang_123
Contributor II

There is currently a project using MMA6827, can we provide the following M driver library files?

0 Kudos
Reply
3 Replies

1,781 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eric,

for a reference driver to the MMA68xx, please refer to this community thread. There is a link to TWR_SENSOR_AUTO_FW package.
Please also refer to this community thread and also to this one. It might be useful for you.

With Best Regards,

Jozef

0 Kudos
Reply

1,741 Views
Zhang_123
Contributor II

Thank you very much for your previous answer. I wonder if the MM6827 can set the range and sensitivity? I didn't see the specific register, thank you very much!

1,735 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Eric,

I wonder if the MM6827 can set the range and sensitivity? I didn't see the specific register.

[A] Unfortunately no. The MMA6827 accelerometer and other MMA68xx accelerometers range and sensitivity cannot be changed. If you need accelerometer with different range, you can chose other one from the same family. Please refer to the Table in the page 1, and to section 3.4 in the MMA68xx datasheet.

JozefKozon_0-1679640330688.pngJozefKozon_1-1679640361377.png


With Best Regards,

Jozef

0 Kudos
Reply