Hi,
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) i.MXRT106 must work with Alexa?
-- No, NXP also provides the local voice recognition solution.
https://www.nxp.com/design/designs/nxp-edgeready-mcu-based-solution-for-local-voice-control:MCU-LOCA...
2) How to input the voice command? It can accept.TXT file? Or Speak input only?
-- Speak is the only way to input the command.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------