MIMXRT106L Voice Solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT106L Voice Solution

1,030件の閲覧回数
lizboxy
Contributor I

Pls confirm some question as:

1. i.MXRT106 must work with Alexa?

2. How to input the voice command?  It can accept with .TXT file? Or Speek input only?

TKs!

0 件の賞賛
返信
1 返信

1,022件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) i.MXRT106 must work with Alexa?
-- No, NXP also provides the local voice recognition solution.
https://www.nxp.com/design/designs/nxp-edgeready-mcu-based-solution-for-local-voice-control:MCU-LOCA...
2) How to input the voice command? It can accept.TXT file? Or Speak input only?
-- Speak is the only way to input the command.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信