MFR4310 Using Flexray Controller as non-coldstart Node

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFR4310 Using Flexray Controller as non-coldstart Node

1,292件の閲覧回数
jochengerster
NXP Employee
NXP Employee

Hello

customer has a problem using MFR4310 as non-coldstart Node - see below more details

Thanks for your help

best regards

Jochen

-------------

"MFR4310" Flexray Controller to transmit Flexray frames.

 

The node I am trying to simulate is:

  • Non-coldstart node.
  • Has 0 Tx static frames.

I used the controller many times to simulate cold start nodes. This is the first time to use it as non-cold start node. I can not get it working.

 

Steps:

  • Initialize registers 0 to 0x2000 to zeros
  • Disable Interrupts through clear "GIFER:MIE_ENABLE" bit
  • Configure to Channel A through setting "MCR:ENABLE_CH_A" bit
  • Enabling the "MCR:MEN" bit
  • Write Command "POCR_CMD:DEFAULT_CONFIG"
  • psr0 indicates "PROTSTATE_DEFAULT:CONFIG"
  • Write Command "POCR_CMD:CONFIG"
  • Configure "PCR0 - PCR31"
  • Initialize all msg-buffers
  • Gifer set: MIE_ENABLE  | PRIE_ENABLE | WUPIE | CHIE
  • POCR_CMD:READY
  • After powering up two external cold startup nodes, I can see their frames on CANoe:
    • POCR_CMD:RUN

Reading PSR0, I find that the Controller is alternating between the states:

  • Integration Listen
  • Init Schedule

I never go to states "POC:integration consistency check" or Enter operation. Of course I can not send any Frames.

 

Is there anything missing?

タグ(1)
0 件の賞賛
返信
0 返答(返信)