MCUXpresso Software cannot recompile bin file with same hash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Software cannot recompile bin file with same hash

801 Views
BetoGreen
Contributor III
Cant seem to ask question on MCUXpresso Software and Tools / MCUXpresso General as no option so I'm posting here. I have an NXP LPC project that I zipped up including bin files and I am trying 1 year later to recompile the project and I don't seem to get the same bin files. Is there a date or something the compiler changed that is different or maybe some references for error handing? Is there a way I can set up my configuration so that I can at any time later compile the same project and generate the same bin file with the same hash?
0 Kudos
Reply
1 Reply

777 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello BetoGreen,

Normally if the build enviroments are the same, the generated bin file should be same as well.

Could you please check if the MCUXpresso version and SDK version changed?

Best Regards

Jun Zhang 

0 Kudos
Reply