MC33774 internal overcurrent data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33774 internal overcurrent data

2,100件の閲覧回数
Louis1916
Contributor III

The customer wants to know what is the maximum overcurrent of the MC33774 VDDC and GPIO internal protection tubes? The data sheet did not find any relevant information.Thanks!

0 件の賞賛
返信
3 返答(返信)

2,067件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Louis,

please see below an answer from an application engineer I have contacted.

DESCRIPTION

The MC33774 VDDC current limitation is given by the Vtrig(VDDC)oc parameter and the Rsense resistor. Above 264mV in the sense resistor can trigger an OC event.

What do you mean by GPIO internal protection tubes ?

With Best Regards,

Jozef

0 件の賞賛
返信

2,027件の閲覧回数
Louis1916
Contributor III

Dear Jozef

  I mean that in addition to the power pin, the internal protection of the other ordinary IO ports can be too current? Thanks!

0 件の賞賛
返信

2,013件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Louis,

unfortunately we do not have this value. The GPIO pins are suppose to be supplied from VDDC or VAUX, depending which regulator is assigned. The maximum current capabilities can be found in the MC33774A full datasheet, but both VDDA and VAUX also supply other circuits, so these are also not relevant values. 

I apologize for inconvenience. 

With Best Regards,

Jozef

0 件の賞賛
返信