MC33771C and MC33772C safety margin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771C and MC33772C safety margin

Jump to solution
1,447 Views
nxf61247
NXP Employee
NXP Employee

       The thresholds (thresholds for mechanisms such as SM03, SM04, and SM07) provided in the datasheet (MC33772B Rev6.0 6/April/2020) and safety manual (MC33772B VerE 4/7/2021) have not undergone EMC or some noise testing, which is also reasonable. Because customers have different requirements for these noises or EMC. Because the threshold range is very narrow, it is very susceptible to external noise from the entire vehicle. The customer has actually reported several cases where these mechanisms incorrectly reported diagnostic results.

     Based on the above issue with MC33772B, it is also necessary to provide the threshold corresponding to the safety margin of 50mV and 100mV for MC33771C and MC33772C.  To avoid customers receiving incorrect diagnostic results in the event of high vehicle noise or EMC.

    Please assist in providing this data. Thank you very much!

 

MC33772B safety margin 

#MC33771C

#MC33772C

@SavinoLupo 

0 Kudos
Reply
1 Solution
1,319 Views
SavinoLupo
NXP Employee
NXP Employee

Hi Zhihua Xu,

the additional information for MC33771C and MC33772C is in the attached file.

Thanks and regards,

Savino

View solution in original post

4 Replies
1,320 Views
SavinoLupo
NXP Employee
NXP Employee

Hi Zhihua Xu,

the additional information for MC33771C and MC33772C is in the attached file.

Thanks and regards,

Savino

1,306 Views
nxf61247
NXP Employee
NXP Employee

     Got it and thank you for you solving quickly.

0 Kudos
Reply
1,427 Views
guoweisun
NXP TechSupport
NXP TechSupport

This is only public community , for these BMS safety questions internally of NXP you'd better contact with Savino directly.

 

0 Kudos
Reply
1,422 Views
nxf61247
NXP Employee
NXP Employee

Thank you very much for your reminder. I haven't noticed this yet.

0 Kudos
Reply