MC33771C and MC33772C safety margin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC33771C and MC33772C safety margin

跳至解决方案
1,121 次查看
nxf61247
NXP Employee
NXP Employee

       The thresholds (thresholds for mechanisms such as SM03, SM04, and SM07) provided in the datasheet (MC33772B Rev6.0 6/April/2020) and safety manual (MC33772B VerE 4/7/2021) have not undergone EMC or some noise testing, which is also reasonable. Because customers have different requirements for these noises or EMC. Because the threshold range is very narrow, it is very susceptible to external noise from the entire vehicle. The customer has actually reported several cases where these mechanisms incorrectly reported diagnostic results.

     Based on the above issue with MC33772B, it is also necessary to provide the threshold corresponding to the safety margin of 50mV and 100mV for MC33771C and MC33772C.  To avoid customers receiving incorrect diagnostic results in the event of high vehicle noise or EMC.

    Please assist in providing this data. Thank you very much!

 

MC33772B safety margin 

#MC33771C

#MC33772C

@SavinoLupo 

0 项奖励
1 解答
993 次查看
SavinoLupo
NXP Employee
NXP Employee

Hi Zhihua Xu,

the additional information for MC33771C and MC33772C is in the attached file.

Thanks and regards,

Savino

在原帖中查看解决方案

4 回复数
994 次查看
SavinoLupo
NXP Employee
NXP Employee

Hi Zhihua Xu,

the additional information for MC33771C and MC33772C is in the attached file.

Thanks and regards,

Savino

980 次查看
nxf61247
NXP Employee
NXP Employee

     Got it and thank you for you solving quickly.

0 项奖励
1,101 次查看
guoweisun
NXP TechSupport
NXP TechSupport

This is only public community , for these BMS safety questions internally of NXP you'd better contact with Savino directly.

 

0 项奖励
1,096 次查看
nxf61247
NXP Employee
NXP Employee

Thank you very much for your reminder. I haven't noticed this yet.

0 项奖励