LS1088A design without CPLD device ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1088A design without CPLD device ?

1,258 Views
toidong
Contributor I

Dear Experts,

We have a project with LS1088A processor and EPM2210F256C5N as a CPLD device,

So,

1. Can we design LS1088A without a CPLD device?

2. If YES, can you give me a guideline or reference design?

3. If No, can you give some other part number of the CPLD device at a lower cost ?

4. We're going to use 10M08SAU169C8G as a low-cost CPLD solution, is it ok?

Thank you,

Tags (1)
0 Kudos
Reply
2 Replies

1,226 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. In theory, it is possible.

2. We don't have the reference design.

3. You need to contact the CPLD manufactory for CPLD device list at a lower cost.

4. Please download Design File for LS1088ARDB-PB to get the CPLD source code.

https://www.nxp.com/downloads/en/printed-circuit-boards/LS1088ARDB-PB-DF.zip

Then check whether your CPLD can implement the same functions.

0 Kudos
Reply

1,194 Views
toidong
Contributor I

Hi @yipingwang ,

I got the answers, thanks so much for your support

0 Kudos
Reply