LS1046ardb failed to load with initramfs packed with fitImage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046ardb failed to load with initramfs packed with fitImage

578 次查看
prafulls
Contributor II

Hi Team,

   We were using the LS1046ardb & will need to load the fitImage with initramfs , we have packed the ramdisk in fitImage using yocto 3.1. but it fail to load with initramfs. Can you suggest the right procedure  to this , please find below console logs for reference.

 

NOTICE: 8 GB DDR4, 64-bit, CL=15, ECC off
NOTICE: BL2: v1.5(release):LSDK-20.04-update-290520-3-g31fdcadba-dirty
NOTICE: BL2: Built : 13:25:49, Aug 4 2021
NOTICE: BL31: v1.5(release):LSDK-20.04-update-290520-3-g31fdcadba-dirty
NOTICE: BL31: Built : 13:25:52, Aug 4 2021
NOTICE: Welcome to LS1046 BL31 Phase


U-Boot 2019.10-00009-g919028d133-dirty (Aug 04 2021 - 13:25:14 +0800)

SoC: LS1046AE Rev1.0 (0x87070010)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz
Bus: 700 MHz DDR: 2100 MT/s FMAN: 800 MHz
Reset Configuration Word (RCW):
00000000: 0e150012 10000000 00000000 00000000
00000010: 13335577 40200012 40045000 c1000000
00000020: 00000000 00000000 00000000 0002c800
00000030: 20004500 28263000 00000096 00000001
Model: LS1046A RDB Board
Board: LS1046ARDB(sw ver1.2.24), boot from QSPI.
GPIO: configure mux to GPIO3_10 GPIO3_11.
DRAM: 7.9 GiB (DDR4, 64-bit, CL=15, ECC off)
SEC0: RNG instantiated
Using SERDES1 Protocol: 4915 (0x1333)
Using SERDES2 Protocol: 21879 (0x5577)
NAND: 0 MiB
MMC: FSL_SDHC: 0
Loading Environment from SPI Flash... SF: Detected mx25u51245g with page size 2
56 Bytes, erase size 64 KiB, total 64 MiB
OK
EEPROM: Read failed.
In: serial
Out: serial
Err: serial
Net: SF: Detected mx25u51245g with page size 256 Bytes, erase size 64 KiB, to
tal 64 MiB
Fman1: Uploading microcode version 106.4.18
marvell phy enable synce.
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 disabled
PCIe2: pcie@3600000 Root Complex
DSPI: Send spi command successfully.
: x2 gen2
FM1@DTSEC6 [PRIME], FM1@DTSEC10, FM1@TGEC1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
Loading from Yocto fitImage...!!
19517648 bytes read in 944 ms (19.7 MiB/s)
## Loading kernel from FIT Image at a0000000 ...
Using 'conf@freescale_fsl-ls1046a-rdb-usdpaa-shared.dtb' configuration
Trying 'kernel@1' kernel subimage
Description: Linux kernel
Type: Kernel Image
Compression: gzip compressed
Data Start: 0xa0000110
Data Size: 15386559 Bytes = 14.7 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x80080000
Entry Point: 0x80080000
Hash algo: sha256
Hash value: e9027d5154dfdd9d917afb1cd133cd671d14f1076c7e882374e59d80be2c
6293
Verifying Hash Integrity ... sha256+ OK
## Loading ramdisk from FIT Image at a0000000 ...
Using 'conf@freescale_fsl-ls1046a-rdb-usdpaa-shared.dtb' configuration
Trying 'ramdisk@1' ramdisk subimage
Description: core-image-cpe-minimal-initramfs
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0xa0ee3fe8
Data Size: 3901295 Bytes = 3.7 MiB
Architecture: AArch64
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Hash algo: sha256
Hash value: 4515f7e37602343089f402f8d3fe720a1c8553b42e678c28013e1180764f
03ad
Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at a0000000 ...
Using 'conf@freescale_fsl-ls1046a-rdb-usdpaa-shared.dtb' configuration
Trying 'fdt@freescale_fsl-ls1046a-rdb-usdpaa-shared.dtb' fdt subimage
Description: Flattened Device Tree blob
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0xa0eac9fc
Data Size: 41262 Bytes = 40.3 KiB
Architecture: AArch64
Load Address: 0x90000000
Hash algo: sha256
Hash value: caf2a3bc1629d2f6291060a92e37a7f8451d9cae7735d49c6f8596fc8b5b
cad2
Verifying Hash Integrity ... sha256+ OK
Loading fdt from 0xa0eac9fc to 0x90000000
Booting using the fdt blob at 0x90000000
Uncompressing Kernel Image
Using Device Tree in place at 0000000090000000, end 000000009001d12d

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd082]
[ 0.000000] Linux version 4.19.90-rt35+g134788b16485 (oe-user@oe-host) (gcc
version 9.3.0 (GCC)) #1 SMP PREEMPT RT Mon May 25 09:38:43 UTC 2020
[ 0.000000] Machine model: LS1046A RDB Board
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
[ 0.000000] bootconsole [uart8250] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: initialized node qman-fqd, compatible id fsl,q
man-fqd
[ 0.000000] OF: reserved mem: initialized node qman-pfdr, compatible id fsl,
qman-pfdr
[ 0.000000] OF: reserved mem: initialized node usdpaa_mem, compatible id fsl
,usdpaa-mem
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,
bman-fbpr
[ 0.000000] cma: Reserved 32 MiB at 0x00000000f9c00000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000009ff7ffff
f]
[ 0.000000] NUMA: NODE_DATA [mem 0x9ff7b7f00-0x9ff7b973f]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] Normal [mem 0x0000000100000000-0x00000009ff7fffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000009fbffffff]
[ 0.000000] node 0: [mem 0x00000009ff000000-0x00000009ff7fffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000009ff7fffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] random: get_random_bytes called from start_kernel+0x9c/0x480 wit
h crng_init=0
[ 0.000000] percpu: Embedded 26 pages/cpu s67008 r8192 d31296 u106496
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for EL2 vector hardening
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 2033376
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyS0,115200 root=/dev/mmcblk0p6 rd
init=/init earlycon=uart8250,mmio,0x21c0500 mtdparts=1550000.spi-0:1m(rcw),15m(
u-boot),48m(kern)
[ 0.000000] software IO TLB: mapped [mem 0xf5c00000-0xf9c00000] (64MB)
[ 0.000000] Memory: 7730380K/8263680K available (16060K kernel code, 2690K r
wdata, 6548K rodata, 10368K init, 1001K bss, 500532K reserved, 32768K cma-reser
ved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] ftrace: allocating 53988 entries in 211 pages
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x000000000142f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] rcu: Offload RCU callbacks from CPUs: (none).
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles
: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000001] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398
046511100ns
[ 0.000287] Console: colour dummy device 80x25
[ 0.314753] Calibrating delay loop (skipped), value calculated using timer f
requency.. 50.00 BogoMIPS (lpj=100000)
[ 0.314756] pid_max: default: 32768 minimum: 301
[ 0.314788] Security Framework initialized
[ 0.319403] Dentry cache hash table entries: 1048576 (order: 12, 16777216 by
tes)
[ 0.324733] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes
)
[ 0.324796] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.324837] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 byt
es)
[ 0.348169] ASID allocator initialised with 32768 entries
[ 0.416193] rcu: Hierarchical SRCU implementation.
[ 0.446344] EFI services will not be available.
[ 0.456239] smp: Bringing up secondary CPUs ...
[ 0.516380] Detected PIPT I-cache on CPU1
[ 0.516406] CPU1: Booted secondary processor 0x0000000001 [0x410fd082]
[ 0.572413] Detected PIPT I-cache on CPU2
[ 0.572426] CPU2: Booted secondary processor 0x0000000002 [0x410fd082]
[ 0.628466] Detected PIPT I-cache on CPU3
[ 0.628479] CPU3: Booted secondary processor 0x0000000003 [0x410fd082]
[ 0.628515] smp: Brought up 1 node, 4 CPUs
[ 0.664369] SMP: Total of 4 processors activated.
[ 0.669094] CPU features: detected: 32-bit EL0 Support
[ 0.674591] CPU: All CPU(s) started at EL2
[ 0.678717] alternatives: patching kernel code
[ 0.679337] devtmpfs: initialized
[ 0.691572] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, m
ax_idle_ns: 7645041785100000 ns
[ 0.701399] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.708053] xor: measuring software checksum speed
[ 0.752493] 8regs : 7029.000 MB/sec
[ 0.796520] 8regs_prefetch: 6252.000 MB/sec
[ 0.840548] 32regs : 8071.000 MB/sec
[ 0.884572] 32regs_prefetch: 7033.000 MB/sec
[ 0.889208] xor: using function: 32regs (8071.000 MB/sec)
[ 0.894633] pinctrl core: initialized pinctrl subsystem
[ 0.900680] DMI not present or invalid.
[ 0.904797] NET: Registered protocol family 16
[ 0.909441] audit: initializing netlink subsys (disabled)
[ 0.914935] audit: type=2000 audit(0.912:1): state=initialized audit_enabled
=0 res=1
[ 0.916003] cpuidle: using governor ladder
[ 0.916077] NET: Registered protocol family 42
[ 0.916136] Bman ver:0a02,02,01
[ 0.918061] qman-fqd addr 0x00000009ff800000 size 0x800000
[ 0.918064] qman-pfdr addr 0x00000009fc000000 size 0x2000000
[ 0.918076] Qman ver:0a01,03,02,01
[ 0.918220] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval__
__))
[ 0.918223] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.921536] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.922129] Serial: AMBA PL011 UART driver
[ 0.928344] Machine: LS1046A RDB Board
[ 0.928346] SoC family: QorIQ LS1046A
[ 0.928348] SoC ID: svr:0x87070010, Revision: 1.0
[ 0.949929] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 1.016783] raid6: int64x1 gen() 1118 MB/s
[ 1.088830] raid6: int64x1 xor() 1012 MB/s
[ 1.160878] raid6: int64x2 gen() 1521 MB/s
[ 1.232913] raid6: int64x2 xor() 1449 MB/s
[ 1.304981] raid6: int64x4 gen() 2078 MB/s
[ 1.377012] raid6: int64x4 xor() 1597 MB/s
[ 1.449087] raid6: int64x8 gen() 2515 MB/s
[ 1.521117] raid6: int64x8 xor() 1574 MB/s
[ 1.593174] raid6: neonx1 gen() 2303 MB/s
[ 1.665198] raid6: neonx1 xor() 2450 MB/s
[ 1.737257] raid6: neonx2 gen() 2895 MB/s
[ 1.809293] raid6: neonx2 xor() 3108 MB/s
[ 1.881352] raid6: neonx4 gen() 3365 MB/s
[ 1.953382] raid6: neonx4 xor() 3126 MB/s
[ 2.025427] raid6: neonx8 gen() 3972 MB/s
[ 2.097472] raid6: neonx8 xor() 3624 MB/s
[ 2.101758] raid6: using algorithm neonx8 gen() 3972 MB/s
[ 2.107181] raid6: .... xor() 3624 MB/s, rmw enabled
[ 2.112166] raid6: using neon recovery algorithm
[ 2.117245] ACPI: Interpreter disabled.
[ 2.122528] vgaarb: loaded
[ 2.125399] SCSI subsystem initialized
[ 2.129500] usbcore: registered new interface driver usbfs
[ 2.135036] usbcore: registered new interface driver hub
[ 2.140407] usbcore: registered new device driver usb
[ 2.146557] imx-i2c 2190000.i2c: scl-gpios not found
[ 2.151650] i2c i2c-0: IMX I2C adapter registered
[ 2.157113] pps_core: LinuxPPS API ver. 1 registered
[ 2.162107] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom
etti <giometti@linux.it>
[ 2.171298] PTP clock support registered
[ 2.175396] EDAC MC: Ver: 3.0.0
[ 2.178789] bman-fbpr addr 0x00000009fe000000 size 0x1000000
[ 2.184557] Bman err interrupt handler present
[ 2.189573] Bman portal initialised, cpu 0
[ 2.193837] Bman portal initialised, cpu 1
[ 2.198090] Bman portal initialised, cpu 2
[ 2.202349] Bman portal initialised, cpu 3
[ 2.206460] Bman portals initialised
[ 2.210862] Qman err interrupt handler present
[ 2.215890] QMan: Allocated lookup table at (____ptrval____), entry count 13
1073
[ 2.223815] Qman portal initialised, cpu 0
[ 2.228072] Qman portal initialised, cpu 1
[ 2.232330] Qman portal initialised, cpu 2
[ 2.236589] Qman portal initialised, cpu 3
[ 2.240713] Qman portals initialised
[ 2.244368] Bman: BPID allocator includes range 16:48
[ 2.249479] Qman: FQID allocator includes range 256:256
[ 2.254728] Qman: FQID allocator includes range 32768:32768
[ 2.260366] Qman: CGRID allocator includes range 0:256
[ 2.265661] Qman: pool channel allocator includes range 1025:15
[ 2.271685] USDPAA region at 9e0000000:10000000(9e0000:10000), 1 TLB1 entrie
s)
[ 2.279341] fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller
[ 2.285927] fsl-ifc 1530000.ifc: IFC version 1.4, 8 banks
[ 2.292121] clocksource: Switched to clocksource arch_sys_counter
[ 2.340624] VFS: Disk quotas dquot_6.6.0
[ 2.344601] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 2.351638] pnp: PnP ACPI: disabled
[ 2.359892] NET: Registered protocol family 2
[ 2.364664] tcp_listen_portaddr_hash hash table entries: 4096 (order: 6, 262
144 bytes)
[ 2.372894] TCP established hash table entries: 65536 (order: 7, 524288 byte
s)
[ 2.381051] TCP bind hash table entries: 65536 (order: 9, 3670016 bytes)
[ 2.389232] TCP: Hash tables configured (established 65536 bind 65536)
[ 2.396156] UDP hash table entries: 4096 (order: 7, 524288 bytes)
[ 2.402625] UDP-Lite hash table entries: 4096 (order: 7, 524288 bytes)
[ 2.409522] NET: Registered protocol family 1
[ 2.414186] RPC: Registered named UNIX socket transport module.
[ 2.420258] RPC: Registered udp transport module.
[ 2.424982] RPC: Registered tcp transport module.
[ 2.429706] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 2.465209] Trying to unpack rootfs image as initramfs...
[ 2.586641] Freeing initrd memory: 3808K
[ 2.591013] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 count
ers available
[ 2.599544] kvm [1]: 8-bit VMID
[ 2.603128] kvm [1]: vgic interrupt IRQ1
[ 2.607126] kvm [1]: Hyp mode initialized successfully
[ 2.613867] workingset: timestamp_bits=44 max_order=21 bucket_order=0
[ 2.624992] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 2.631263] NFS: Registering the id_resolver key type
[ 2.636347] Key type id_resolver registered
[ 2.640546] Key type id_legacy registered
[ 2.644578] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 2.651415] fuse init (API version 7.27)
[ 2.655587] 9p: Installing v9fs 9p2000 file system support
[ 2.662987] Block layer SCSI generic (bsg) driver version 0.4 loaded (major
244)
[ 2.670493] io scheduler noop registered
[ 2.674431] io scheduler deadline registered
[ 2.678799] io scheduler cfq registered (default)
[ 2.683523] io scheduler mq-deadline registered
[ 2.688073] io scheduler kyber registered
[ 2.703671] ls_pcie_probe: NXP board 0, dbi_base (____ptrval____) can_force
3 0
[ 2.711029] layerscape-pcie 3600000.pcie: host bridge /soc/pcie@3600000 rang
es:
[ 2.718388] layerscape-pcie 3600000.pcie: IO 0x5000010000..0x500001ffff -
> 0x00000000
[ 2.726526] layerscape-pcie 3600000.pcie: MEM 0x5040000000..0x507fffffff -
> 0x40000000
[ 2.734770] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0000:00
[ 2.741508] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.747020] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 2.753231] pci_bus 0000:00: root bus resource [mem 0x5040000000-0x507ffffff
f] (bus address [0x40000000-0x7fffffff])
[ 2.765816] pci 0000:01:00.0: 8.000 Gb/s available PCIe bandwidth, limited b
y 5 GT/s x2 link at 0000:00:00.0 (capable of 15.752 Gb/s with 8 GT/s x2 link)
[ 2.789273] pci 0000:00:00.0: BAR 14: assigned [mem 0x5040000000-0x50400ffff
f]
[ 2.796535] pci 0000:00:00.0: BAR 6: assigned [mem 0x5040100000-0x50401007ff
pref]
[ 2.804152] pci 0000:01:00.0: BAR 0: assigned [mem 0x5040000000-0x5040000fff
64bit]
[ 2.811882] pci 0000:01:00.0: BAR 2: assigned [mem 0x5040001000-0x5040001fff
64bit]
[ 2.819610] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 2.824860] pci 0000:00:00.0: bridge window [mem 0x5040000000-0x50400fffff
]
[ 2.834146] EINJ: ACPI disabled.
[ 2.843407] Freescale LS2 console driver
[ 2.847423] fsl-ls2-console: device fsl_mc_console registered
[ 2.853263] fsl-ls2-console: device fsl_aiop_console registered
[ 2.864747] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 2.873060] console [ttyS0] disabled
[ 2.876692] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 42, base_baud = 2
1875000) is a 16550A
[ 2.885547] console [ttyS0] enabled
[ 2.885547] console [ttyS0] enabled
[ 2.892524] bootconsole [uart8250] disabled
[ 2.892524] bootconsole [uart8250] disabled
[ 2.901280] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 42, base_baud = 2
1875000) is a 16550A
[ 2.910662] SuperH (H)SCI(F) driver initialized
[ 2.915723] msm_serial: driver initialized
[ 2.921595] FSM-TTI: probing device
[ 2.925285] FSM-TTI: cdev initialized
[ 2.928953] FSM-TTI: debugfs initialized
[ 2.932867] FSM-TTI: module initialized
[ 2.936957] arm-smmu 9000000.iommu: probing hardware configuration...
[ 2.943392] arm-smmu 9000000.iommu: SMMUv2 with:
[ 2.948002] arm-smmu 9000000.iommu: stage 1 translation
[ 2.953306] arm-smmu 9000000.iommu: stage 2 translation
[ 2.958611] arm-smmu 9000000.iommu: nested translation
[ 2.963828] arm-smmu 9000000.iommu: coherent table walk
[ 2.969133] arm-smmu 9000000.iommu: stream matching with 64 register groups
[ 2.976178] arm-smmu 9000000.iommu: 32 context banks (0 stage-2 only)
[ 2.982700] arm-smmu 9000000.iommu: Supported page sizes: 0x61311000
[ 2.989134] arm-smmu 9000000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 2.995568] arm-smmu 9000000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 3.008293] brd: module loaded
[ 3.016509] loop: module loaded
[ 3.023540] fsl-quadspi 1550000.spi: mx66u51235f (65536 Kbytes)
[ 3.033622] libphy: Fixed MDIO Bus: probed
[ 3.038359] tun: Universal TUN/TAP device driver, 1.6
[ 3.044429] thunder_xcv, ver 1.0
[ 3.047677] thunder_bgx, ver 1.0
[ 3.050921] nicpf, ver 1.0
[ 3.053845] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.062437] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.067487] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.073849] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.080218] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.086472] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.093088] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.099381] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.105630] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.111828] libphy: Freescale XGMAC MDIO Bus: probed
[ 3.127129] Freescale FM module, FMD API version 21.1.0
[ 3.133610] iommu: Adding device 1a88000.port to group 0
[ 3.139101] iommu: Adding device 1aa8000.port to group 0
[ 3.144582] iommu: Adding device 1a89000.port to group 0
[ 3.150059] iommu: Adding device 1aa9000.port to group 0
[ 3.155540] iommu: Adding device 1a8a000.port to group 0
[ 3.161015] iommu: Adding device 1aaa000.port to group 0
[ 3.166490] iommu: Adding device 1a8b000.port to group 0
[ 3.171967] iommu: Adding device 1aab000.port to group 0
[ 3.177447] iommu: Adding device 1a8c000.port to group 0
[ 3.182928] iommu: Adding device 1aac000.port to group 0
[ 3.188405] iommu: Adding device 1a8d000.port to group 0
[ 3.193884] iommu: Adding device 1aad000.port to group 0
[ 3.199366] iommu: Adding device 1a90000.port to group 0
[ 3.204852] iommu: Adding device 1ab0000.port to group 0
[ 3.210338] iommu: Adding device 1a91000.port to group 0
[ 3.215817] iommu: Adding device 1ab1000.port to group 0
[ 3.221331] Freescale FM Ports module
[ 3.224985] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 3.230989] fsl_mac 1aea000.ethernet: FMan MEMAC
[ 3.235603] fsl_mac 1aea000.ethernet: FMan MAC address: 24:0b:88:05:54:8b
[ 3.244047] fsl_mac 1af0000.ethernet: FMan MEMAC
[ 3.248661] fsl_mac 1af0000.ethernet: FMan MAC address: 5e:86:dc:70:2f:0f
[ 3.255725] fsl_mac 1af2000.ethernet: FMan MEMAC
[ 3.260337] fsl_mac 1af2000.ethernet: FMan MAC address: 24:0b:88:05:54:8a
[ 3.267182] fsl_dpa: FSL DPAA Ethernet driver
[ 3.276019] fsl_dpa: fsl_dpa: Probed interface eth0
[ 3.285169] fsl_dpa: fsl_dpa: Probed interface eth1
[ 3.294290] fsl_dpa: fsl_dpa: Probed interface eth2
[ 3.299240] fsl_advanced: FSL DPAA Advanced drivers:
[ 3.304197] fsl_proxy: FSL DPAA Proxy initialization driver
[ 3.310000] fsl_oh: FSL FMan Offline Parsing port driver
[ 3.315456] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Found OH node handle compati
ble with fsl,dpa-oh
[ 3.324194] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Allocating 0 ingress frame q
ueues duples
[ 3.332366] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: OH port port@83000 has no bu
ffer pool. Fragmentation will not be enabled
[ 3.343349] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: OH port port@83000 enabled.
[ 3.350305] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Default egress frame queue:
97
[ 3.357521] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Default error frame queue: 9
6
[ 3.364649] fsl_oh soc:fsl,dpaa:dpa-fman0-oh@2: Initialized queues:
[ 3.371841] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 3.378883] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 3.384653] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 3.390478] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 3.396422] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[ 3.403376] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 3.408969] igbvf: Intel(R) Gigabit Virtual Function Network Driver - versio
n 2.4.0-k
[ 3.416792] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 3.423168] sky2: driver version 1.30
[ 3.427633] usbcore: registered new interface driver r8152
[ 3.433133] usbcore: registered new interface driver asix
[ 3.438549] usbcore: registered new interface driver ax88179_178a
[ 3.445136] VFIO - User Level meta-driver version: 0.3
[ 3.451842] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.458371] ehci-pci: EHCI PCI platform driver
[ 3.462831] ehci-platform: EHCI generic platform driver
[ 3.468245] ehci-orion: EHCI orion driver
[ 3.472387] ehci-exynos: EHCI EXYNOS driver
[ 3.476690] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 3.482870] ohci-pci: OHCI PCI platform driver
[ 3.487329] ohci-platform: OHCI generic platform driver
[ 3.492698] ohci-exynos: OHCI EXYNOS driver
[ 3.497434] usbcore: registered new interface driver usb-storage
[ 3.505369] udc-core: couldn't find an available UDC - added [g_serial] to l
ist of pending drivers
[ 3.515904] ftm-alarm 29d0000.timer: registered as rtc1
[ 3.522172] i2c /dev entries driver
[ 3.527662] pps pps0: new PPS source ktimer
[ 3.531839] pps pps0: ktimer PPS source registered
[ 3.536624] pps_ldisc: PPS line discipline registered
[ 3.541931] pps pps1: new PPS source pps.-1
[ 3.546187] pps pps1: Registered IRQ 71 as PPS source
[ 3.551673] ptp_qoriq: device tree node missing required elements, try autom
atic configuration
[ 3.560278] ptp_qoriq: ptp_qoriq_auto_config: set ref clock as 0
[ 3.566277] ptp_qoriq: ptp_qoriq_auto_config, working frequency of 1588IP is
100000000
[ 3.574276] ptp_qoriq: ptp_qoriq_init: set ref clock as 0
[ 3.579816] pps pps2: new PPS source ptp0
[ 3.583839] ptp_qoriq: ---->found 1 GPIOS defined in DT
[ 3.589088] ptp_qoriq: port write takes 297ns
[ 3.596889] imx2-wdt 2ad0000.watchdog: timeout 60 sec (nowayout=0)
[ 3.604513] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 3.611662] sdhci: Secure Digital Host Controller Interface driver
[ 3.617835] sdhci: Copyright(c) Pierre Ossman
[ 3.622597] Synopsys Designware Multimedia Card Interface Driver
[ 3.629837] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.636042] iommu: Adding device 1560000.esdhc to group 1
[ 3.667308] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using AD
MA 64-bit
[ 3.677275] iommu: Adding device 1700000.crypto to group 0
[ 3.683002] caam 1700000.crypto: Linux CAAM Queue I/F driver initialised
[ 3.692231] caam 1700000.crypto: device ID = 0x0a11030100000000 (Era
[ 3.698846] caam 1700000.crypto: job rings = 3, qi = 1
[ 3.704481] iommu: Adding device 1710000.jr to group 2
[ 3.714343] caam algorithms registered in /proc/crypto
[ 3.720462] caam 1700000.crypto: caam pkc algorithms registered in /proc/cry
pto
[ 3.728205] caam_jr 1710000.jr: registering rng-caam
[ 3.736713] caam 1700000.crypto: algorithms registered in /proc/crypto
[ 3.743323] iommu: Adding device 1720000.jr to group 3
[ 3.748863] iommu: Adding device 1730000.jr to group 4
[ 3.754964] usbcore: registered new interface driver usbhid
[ 3.760530] usbhid: USB HID core driver
[ 3.764605] iommu: Adding device 1890000.bman to group 5
[ 3.770284] iommu: Adding device 1880000.qman to group 6
[ 3.771633] mmc0: new HS200 MMC card at address 0001
[ 3.772288] mmcblk0: mmc0:0001 008GB0 7.28 GiB
[ 3.772722] mmcblk0boot0: mmc0:0001 008GB0 partition 1 4.00 MiB
[ 3.773173] mmcblk0boot1: mmc0:0001 008GB0 partition 2 4.00 MiB
[ 3.773297] mmcblk0rpmb: mmc0:0001 008GB0 partition 3 4.00 MiB, chardev (509
:0)
[ 3.782922] mmcblk0: p1 p2 p3 p4 < p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p
16 p17 p18 p19 p20 p21 >
[ 3.813874] Freescale USDPAA process driver
[ 3.818123] Freescale USDPAA process IRQ driver
[ 3.825166] optee: probing for conduit method from DT.
[ 3.830299] optee: api uid mismatch
[ 3.834008] u32 classifier
[ 3.836706] Actions configured
[ 3.841026] Initializing XFRM netlink socket
[ 3.845577] NET: Registered protocol family 10
[ 3.850577] Segment Routing with IPv6
[ 3.854280] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.860492] NET: Registered protocol family 17
[ 3.864939] NET: Registered protocol family 15
[ 3.869400] Bridge firewalling registered
[ 3.873468] 8021q: 802.1Q VLAN Support v1.8
[ 3.877728] 9pnet: Installing 9P2000 support
[ 3.882012] tsn generic netlink module v1 init...
[ 3.886739] Key type dns_resolver registered
[ 3.891422] registered taskstats version 1
[ 3.896322] Btrfs loaded, crc32c=crc32c-generic
[ 3.902613] iommu: Adding device 2c00000.edma to group 7
[ 3.910047] i2c i2c-1: using dma0chan16 (tx) and dma0chan17 (rx) for DMA tra
nsfers
[ 3.917614] i2c i2c-1: IMX I2C adapter registered
[ 3.922389] iommu: Adding device 0000:00:00.0 to group 8
[ 3.927904] pcieport 0000:00:00.0: Signaling PME with IRQ 67
[ 3.933638] iommu: Adding device 0000:01:00.0 to group 8
[ 3.939193] mhi 0000:01:00.0: BAR 0: assigned [mem 0x5040000000-0x5040000fff
64bit]
[ 3.947147] [I][mhi_async_power_up] Requested to power on
[ 3.953473] [I][mhi_async_power_up] Power on setup success
[ 3.958964] [I][mhi_pci_probe] Return successful
[ 3.963604] [I][mhi_fw_load_worker] Waiting for device to enter PBL from EE:
INVALID_EE
[ 3.964150] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 3.964302] hctosys: unable to open rtc device (rtc0)
[ 3.964529] Warning: unable to open an initial console.
[ 3.972501] Freeing unused kernel memory: 10368K
[ 3.972576] Run /init as init process
[ 3.996739] [I][mhi_pm_st_worker] Transition to state:PBL
[ 4.002141] [I][mhi_runtime_idle] Entered returning -EBUSY
[ 4.007630] [I][mhi_fw_load_worker] Device current EE:PBL
[ 4.013065] mhi 0000:01:00.0: Direct firmware load for fsm100xx/sbl1.mbn fai
led with error -2
[ 4.021589] [E][mhi_fw_load_worker] Error loading firmware, ret:-2
[ 4.094640] sysrq: SysRq : Keyboard mode set to system default
[ 6.102045] sysrq: SysRq : Emergency Sync
[ 6.106101] Emergency Sync complete
[ 8.109660] sysrq: SysRq : Emergency Remount R/O
[ 8.114293] Emergency Remount complete
[ 8.120432] sysrq: SysRq : Resetting

NOTICE: 8 GB DDR4, 64-bit, CL=15, ECC off
NOTICE: BL2: v1.5(release):LSDK-20.04-update-290520-3-g31fdcadba-dirty
NOTICE: BL2: Built : 13:25:49, Aug 4 2021
NOTICE: BL31: v1.5(release):LSDK-20.04-update-290520-3-g31fdcadba-dirty
NOTICE: BL31: Built : 13:25:52, Aug 4 2021
NOTICE: Welcome to LS1046 BL31 Phase

Thanks,

Prafull

0 项奖励
回复
0 回复数