LS1046 TMU clock config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 TMU clock config

1,109件の閲覧回数
yirw
Contributor I

In the LS146ARM Clocking chapter, the clock for TMU is 1/2 Platform Clock. Clock enablements such as spi, i2c, gpio, etc. are configured in the DEVDISR register of Chapter 12 “Device Configuration and Pin Control”, but no TMU related configuration bit is found. How should the TMU clock be configured? Thank you!

0 件の賞賛
返信
1 返信

1,092件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @yirw,

A given application may not use all the peripherals on the device. In that case, it may be desirable to disable unused peripherals. DEVDISR provides a mechanism for gating clocks to IP blocks that are not used when running an application.
You can enable/disable the TMU monitoring mode by configuring TMR[ME] mode bit. Please refer to chapter# 33 in the LS1046ARM for more details.

Regards,
Mrudang

0 件の賞賛
返信