LS1046 TMU clock config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 TMU clock config

1,103 Views
yirw
Contributor I

In the LS146ARM Clocking chapter, the clock for TMU is 1/2 Platform Clock. Clock enablements such as spi, i2c, gpio, etc. are configured in the DEVDISR register of Chapter 12 “Device Configuration and Pin Control”, but no TMU related configuration bit is found. How should the TMU clock be configured? Thank you!

0 Kudos
Reply
1 Reply

1,086 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @yirw,

A given application may not use all the peripherals on the device. In that case, it may be desirable to disable unused peripherals. DEVDISR provides a mechanism for gating clocks to IP blocks that are not used when running an application.
You can enable/disable the TMU monitoring mode by configuring TMR[ME] mode bit. Please refer to chapter# 33 in the LS1046ARM for more details.

Regards,
Mrudang

0 Kudos
Reply