LS1043A Clarifications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A Clarifications

1,204件の閲覧回数
Akshayv
Contributor II

HI,

was having some doubts regarding LS1043A.

1. In the datasheet it clearly detailed about the power on sequencing of LS1043A. Nothing is given in the datasheet regarding the power down sequencing. what should be the power down procedure for LS1043A. which all rails should be powered down in what sequence..?

2. We have chosen MC34VR500V4ES as the PMIC for power on sequencing LS1043A as per the NXP reference designs. the power down sequencing of this PMIC is disabling all rails at the same time. Will this be appropriate to such a processor to shut down without a proper sequence..? Will this PMIC power down affect the processor performance and lifetime..?

2. Regarding the case of USB ID pin of LS1043A, the power for LS1043A USB power section is provided to USB_HVDD(3.3 V) and USB_SVDD, USB_SDD (1.0 V). In the datasheet USB_ID is to be provided as a 1.8 V signal. being an input, we previously provided a 3.3 V to this pin. Should we change this to 1.8 V..?

Earliest reply is appreciated.

 

---

Thanks & Regards,

Akshay V

0 件の賞賛
返信
1 返信

1,188件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) No specific requirements for the rails power down sequence.

2) You wrote:

> Will this be appropriate to such a processor to shut down without a proper sequence..?

Yes.

> Will this PMIC power down affect the processor performance and lifetime..?

No.

2) You wrote:

> Should we change this to 1.8 V..?

Yes.

The permissible voltage range for this input signal is 0 - 1.8 V.

0 件の賞賛
返信