Hi,
bitbake -c menuconfig virtual/bootloader after saving the changes to .config
bitbake -c compile -f virtual/bootloader fails with below error as oe_runmake failed.
fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git/include/config ]; then \
| echo >&2 " /export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git is not clean, please run 'make mrproper'"; \
| echo >&2 " in the '/export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git' directory.";\
| /bin/false; \
| fi;
| /export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git is not clean, please run 'make mrproper'
| in the '/export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git' directory.
| make[1]: *** [/export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git/Makefile:1881: prepare3] Error 1
| make[1]: Leaving directory '/export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/build/ls1028ardb_tfa_SECURE_BOOT_defconfig'
| make: *** [Makefile:177: sub-make] Error 2
| make: Leaving directory '/export/home2/yocto-sdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/u-boot-qoriq/2023.04+AUTOINC+49b102d988+fslgit-r0/git'
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/export/home2/yocto-sdk/sources/meta-qoriq/recipes-bsp/u-boot/u-boot-qoriq_2023.04.bb:do_compile) failed with exit code '1'
I have to bitbake clean and rerun to succeed. I need to enable pci support in the uboot menuconfig. I need to bring up wifi module on pcie2 . Kindly guide how to proceed.
with regards,
Sjane