LS1028A Static IP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A Static IP

1,212件の閲覧回数
Sathian
Contributor II

How to configure Gbe and Switch Port with Static IP in LS1028A.

1. Changes to do in BSP LSDK.

2. In runtime Linux environment.

0 件の賞賛
返信
1 返信

1,201件の閲覧回数
bpe
NXP Employee
NXP Employee

1. Changes to do in BSP LSDK.

For RAMDISK-based rootfs types: See LSDK User Guide Section 4.3.13 for steps to unpack, modify and rebuild rootfs image and the manpage for /etc/network/interfaces  for necessary changes.

For SD/eMMC rootfs: none. All necessary changes can be done in runtime.

2. In runtime Linux environment.

Familiarize yourself with manpages for ifconfig and /etc/network/interfaces.

 

Hope this helps,
Platon

 

0 件の賞賛
返信