LS1028A Static IP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A Static IP

1,216 Views
Sathian
Contributor II

How to configure Gbe and Switch Port with Static IP in LS1028A.

1. Changes to do in BSP LSDK.

2. In runtime Linux environment.

0 Kudos
Reply
1 Reply

1,205 Views
bpe
NXP Employee
NXP Employee

1. Changes to do in BSP LSDK.

For RAMDISK-based rootfs types: See LSDK User Guide Section 4.3.13 for steps to unpack, modify and rebuild rootfs image and the manpage for /etc/network/interfaces  for necessary changes.

For SD/eMMC rootfs: none. All necessary changes can be done in runtime.

2. In runtime Linux environment.

Familiarize yourself with manpages for ifconfig and /etc/network/interfaces.

 

Hope this helps,
Platon

 

0 Kudos
Reply