LPDDR4 for IMX8MPLUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR4 for IMX8MPLUS

1,070 Views
Vighnesh
Contributor I

The Micron MT53E1536M32D4DE-046 AAT:C is a 48Gb (6GB) LPDDR4 DRAM component. Is it technically compatible with the i.MX 8M Plus processor? I'm Facing lot of challenges in my IMX8MPLUS board for LPDDR4 compatibility issues. My board was designed for Dual rank dual channel LPDDR4 with size 32Gbit(4GB). I'm not able to find any LPDDR4 which is in stock. Facing PIN compatibilty issues with other LPDDR4 which is 32Gbit(4GB) but Dual channel single rank. Please help me in this regards. Can I use MT53E1536M32D4DE-046 AAT:C inplace 32Gbit(4GB) LPDDR4.

Tags (1)
0 Kudos
Reply
3 Replies

1,014 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @Vighnesh 

Imx8mp can support MT53E1536M32D4DE-046 AAT:C LPDDR4 without any problem, we have verified this DRAM. And it has two ranks, not 4ranks.

B.R

0 Kudos
Reply

1,008 Views
db16122
Contributor IV

Thanks for confirmation. It seems I make a mistake...

0 Kudos
Reply

1,030 Views
db16122
Contributor IV

it may not use 6GB LPPDR4 to replace current 4GB since 6GB with x32bus will need to have 4CS pin while I.mx8 plus only have 2 CS.

 

0 Kudos
Reply