LPC8N04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC8N04

2,490 次查看
kang1
Contributor I

LPC8N04.jpg

I want to ask what is the use of the plates in the development board wreath in the figure,Debugging programs and downloading programs seem to have nothing to do with it.

0 项奖励
回复
7 回复数

2,485 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, DuKang,

The circuit in the red circle is downloading/debugging circuit, as you know that LPC8N04 has two pins PIO0_10/PIO0_11 as SWD port, with pin 2&4 closed for P7 and P8 jumper, the SWD signals of LPC8N04 is connected to the debugging chip LPC11U35, so you can download/debug the LPC8N04 with usb port of chip LPC11U35.

Hope it can help you

BR

XiangJun Rong

 

 

xiangjun_rong_0-1667358835750.png

 

xiangjun_rong_1-1667359050828.png

 

0 项奖励
回复

2,481 次查看
kang1
Contributor I

Hi,XiangJun Rong:

          Thank you very much for your answer. I also want to ask how to configure the debugging mode of MCUXpresso to download and debug programs through the USB of the development board.

0 项奖励
回复

2,478 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

After you input the USB cable, the PC can identify  the USB port, in the device manager of PC, the NXP LPC11Uxx is found as the following pic.

If you use MCUXpresso tools and click "debug", the LPC11Uxx is fou8nd automatically.

 

BR

XiangJun Rong

 

 

xiangjun_rong_0-1667373001567.png

 

0 项奖励
回复

2,475 次查看
kang1
Contributor I

20221103_1.jpg

I point after debugging. Always wait for background operation???

20221103_2.jpg

0 项奖励
回复

2,473 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

pls check if the jumper are configured correctly, pin 2&4 must be closed  for P7 and P8 jumper.

BR

XiangJun Rong

 

0 项奖励
回复

2,467 次查看
kang1
Contributor I

The jumper has been changed, but the software interface has been stuck here.

20221104_3.jpg20221104_4.jpg

0 项奖励
回复

2,465 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

请拨动一下S1开关,以使LPC8N04被供电。

BR

XiangJun Rong

0 项奖励
回复