LLDP sdk image for cross compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLDP sdk image for cross compiler

1,009件の閲覧回数
ranga_yn
Contributor III

Hello NXP,

currently i am trying to make sdk tool chain  - my LLDP (ls-image-main)is build fine.

but with the below command i am getting.. quemu error. can you let me know how to resolved the same and create stand alone tool-chain 

bitbake ls-image-main -c populate_sdk

 

ERROR: dpdk-module-21.11-r0 do_patch: Applying patch '0001-Makefile-add-makefile.patch' on target directory '/FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/dpdk-module/21.11-r0/git'
CmdError('quilt --quiltrc /FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/dpdk-module/21.11-r0/recipe-sysroot-native/etc/quiltrc push', 0, 'stdout: Applying patch 0001-Makefile-add-makefile.patch
The next patch would delete the file kernel/linux/kni/Kbuild,
which does not exist! Applying it anyway.
patching file kernel/linux/kni/Kbuild
Hunk #1 FAILED at 1.
1 out of 1 hunk FAILED -- rejects in file kernel/linux/kni/Kbuild
patching file kernel/linux/kni/Makefile
Patch 0001-Makefile-add-makefile.patch does not apply (enforce with -f)

stderr: ')
ERROR: Logfile of failure stored in: /FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/dpdk-module/21.11-r0/temp/log.do_patch.2393713
ERROR: Task (/FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/sources/meta-qoriq/recipes-extended/dpdk/dpdk-module_21.11.bb:do_patch) failed with exit code '1'
ERROR: nativesdk-qemu-6.2.0-r0 do_patch: Applying patch '0001-qemu-Reinstated-syscall-emulation-through-libc-via-c.patch' on target directory '/FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/build_lx2160ardb-rev2/tmp/work/x86_64-nativesdk-fslsdk-linux/nativesdk-qemu/6.2.0-r0/qemu-6.2.0'
CmdError('quilt --quiltrc /FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/build_lx2160ardb-rev2/tmp/work/x86_64-nativesdk-fslsdk-linux/nativesdk-qemu/6.2.0-r0/recipe-sysroot-native/etc/quiltrc push', 0, 'stdout: Applying patch 0001-qemu-Reinstated-syscall-emulation-through-libc-via-c.patch
patching file linux-user/main.c
Hunk #1 succeeded at 380 with fuzz 1 (offset 2 lines).
Hunk #2 succeeded at 460 (offset 16 lines).
patching file linux-user/qemu.h
Hunk #1 FAILED at 370.
1 out of 1 hunk FAILED -- rejects in file linux-user/qemu.h
patching file linux-user/syscall.c
Hunk #1 succeeded at 62 with fuzz 1 (offset 6 lines).
Hunk #2 succeeded at 143 with fuzz 2 (offset 30 lines).
Hunk #3 succeeded at 261 (offset 32 lines).
Hunk #4 succeeded at 433 with fuzz 2 (offset 42 lines).
Hunk #5 succeeded at 585 (offset -119 lines).
Hunk #6 FAILED at 778.
Hunk #7 succeeded at 771 (offset -86 lines).
Hunk #8 succeeded at 7027 (offset 699 lines).
1 out of 8 hunks FAILED -- rejects in file linux-user/syscall.c
Patch 0001-qemu-Reinstated-syscall-emulation-through-libc-via-c.patch does not apply (enforce with -f)

stderr: ')
ERROR: Logfile of failure stored in: /FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/build_lx2160ardb-rev2/tmp/work/x86_64-nativesdk-fslsdk-linux/nativesdk-qemu/6.2.0-r0/temp/log.do_patch.2393574
ERROR: Task (virtual:nativesdk:/FSM20056_MP1.12/LINUX/target/nxp-lldp-noship/lldp-v40/sources/poky/meta/recipes-devtools/qemu/qemu_6.2.0.bb:do_patch) failed with exit code '1'

0 件の賞賛
返信
1 返信

986件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The file qemu_6.2.0 does not exist in your environment please check it and erase everything about yocto a start again.

Regards

0 件の賞賛
返信