LLDP over NETCONF in LS1028

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLDP over NETCONF in LS1028

ソリューションへジャンプ
3,222件の閲覧回数
sameer_chouksey
Contributor II

Hello Everyone,

I am using LS1028ARDB boards. I need to get LLDP data over NETCONF from the switches. 

For NETCONF, I run Netopeer2 server in the switch and able to connect through a client. But when I request for "get" from the client I don't see the LLDP related details on the response from the switch. 

I have been able to enable LLDP separately on the switch but don't see LLDP information on the get response from the switch.

Can someone please help me understand how can I fetch the LLDP information using NETCONF commands?? Are there specific filters I should use??

Please point me to right docs if there are any. 

 

Thanks,

Sameer

0 件の賞賛
返信
1 解決策
3,199件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I have reviewed NETCONF code and doc, current version of Real-time-edge don't support getting LLDP data via NETCONF, I have discussed this issue with R&D, they will consider to add the related functions in Real-time-edge sysrepo component.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,185件の閲覧回数
sameer_chouksey
Contributor II

Thanks for confirming it @yipingwang.

In this case, what does NXP suggest for the topology discovery?? Are there some reference examples/docs available for SNMP? Please point me to them. 

Regards,

Sameer 

0 件の賞賛
返信
3,179件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Take Real-time-edge-v2.2 as example, you can refer to "4.1.2.4 Web-based configuration" of user guide,
in the sector of "8. Start topoagent server on the boards supported", it also uses lldpd service for the topology discovery.

Thanks

0 件の賞賛
返信
3,200件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I have reviewed NETCONF code and doc, current version of Real-time-edge don't support getting LLDP data via NETCONF, I have discussed this issue with R&D, they will consider to add the related functions in Real-time-edge sysrepo component.

0 件の賞賛
返信