LDMOS MHT1004N Layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LDMOS MHT1004N Layout

2,020件の閲覧回数
saurabhnerkar
Contributor II

Hi,

I am working power amplifiers using MHT1004N and MHT1008N for cooking applications. I have completed the schematic of the same using ADS 2016. While creating the layout, the software says "There is no layout present for the device model MHT1004N". Whether I have to create a layout for the device using datasheet dimensions or is there any alternate package/model which has layout for the device I am using?

Any help will be appreciated.

Thank you.

ラベル(1)
  • RF

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,804件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Unfortunately we don't have any footprint for this devices.

You have to create footprints by yourself using information from the Datasheet.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,804件の閲覧回数
saurabhnerkar
Contributor II

Hey,

Thank you for your response. I will use the datasheet values and work out a

way.

Regards

Saurabh

On Tue, Feb 28, 2017 at 4:05 PM, andrei.skok <[email protected]>

0 件の賞賛
返信