KW45B41Z82AFtBT Program Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45B41Z82AFtBT Program Flash

901 Views
developer_hidden
Contributor I

I have the following queries on KW45B41Z82AFtBT

1. Can I use UART to flash the firmware into the chip?

2. Can the serial Wire debug line only be used to debug and not flash the firmware?

0 Kudos
Reply
1 Reply

885 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Thank you for contacting NXP support.

Yes is possible to use UART to flash the firmware a tool that can be used for this can be the Secure Provisioning Tool.

And regarding the Serial Wire Debug, you can use this also to flash the firmware is not strictly necessary to debug to use this feature.

Information related to SWD can be found on the Reference Manual Chapter 21.2.1 Serial Wire Debug. And also more details on the following application note.

Please let me know if there is anything else where I can help you.

0 Kudos
Reply