Issue with enabling scp03

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with enabling scp03

2,229件の閲覧回数
elixa
Contributor I

In my board plain communication to se05x working well and now in I am trying to enable scp03 with cmake options -DPTMW_SCP=SCP03_SSS -DPTMW_SE05X_Auth=PlatfSCP03. but facing issues while executing the seTool commands. I have enabled the logs and could see scp Authentication Successfull , but fails with command (seTool getCert 0x21 cert.pem)error

smCom :DEBUG: phNxpEse_Transceive Exit status 0x0
smCom :DEBUG:APDU Rx< (Len=2)
69 82
scp :DEBUG:Inc_CommandCounter value (Len=16)
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 02
sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:6879 Function:sss_se05x_TXn
sss :ERROR:Error in Se05x_API_CheckObjectExists
App :WARN :nxEnsure:'status == kStatus_SSS_Success' failed. At Line:587 Function:ex_sss_entry
App :INFO :ex_sss Finished
App :ERROR:ex_sss_entry Failed

 

0 件の賞賛
返信
2 返答(返信)

2,174件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @elixa ,

 

Seems seTool doesn't support getCert parameter, which version of MW are you referring to?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信

2,209件の閲覧回数
elixa
Contributor I

could someone help what could be wrong here. Also Attaching the debug logs here

0 件の賞賛
返信