Is SGTL5000XNBA3 a drop-in replacement for SGTL5000XNAA3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is SGTL5000XNBA3 a drop-in replacement for SGTL5000XNAA3?

Jump to solution
983 Views
DanKSI
Contributor III

Hi,

I have an existing design using a SGTL5000XNAA3, which is now obsolete.  I see there is the SGTL5000XNBA3, which has the same pinout.  Would switching to the "B" part require a board re-spin or is this a drop-in replacement?

Thanks,

Dan K.

Tags (1)
0 Kudos
Reply
1 Solution
960 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dan,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the SGTL5000XNAA3 device is obsolete.

In this case, you may use the SGTL5000XNBA3 device as a direct replacement.

Please be aware that there is a slight difference between the packages. You may review the package dimensions from the datasheet.

diazmarin09_0-1686334645315.png

 

I hope this information helps.

Regards,

David

View solution in original post

2 Replies
950 Views
DanKSI
Contributor III

That is the exact info I was looking for.

Thanks,

Dan K.

0 Kudos
Reply
961 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dan,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the SGTL5000XNAA3 device is obsolete.

In this case, you may use the SGTL5000XNBA3 device as a direct replacement.

Please be aware that there is a slight difference between the packages. You may review the package dimensions from the datasheet.

diazmarin09_0-1686334645315.png

 

I hope this information helps.

Regards,

David