Is SGTL5000XNBA3 a drop-in replacement for SGTL5000XNAA3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is SGTL5000XNBA3 a drop-in replacement for SGTL5000XNAA3?

跳至解决方案
640 次查看
DanKSI
Contributor III

Hi,

I have an existing design using a SGTL5000XNAA3, which is now obsolete.  I see there is the SGTL5000XNBA3, which has the same pinout.  Would switching to the "B" part require a board re-spin or is this a drop-in replacement?

Thanks,

Dan K.

标记 (1)
0 项奖励
1 解答
617 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dan,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the SGTL5000XNAA3 device is obsolete.

In this case, you may use the SGTL5000XNBA3 device as a direct replacement.

Please be aware that there is a slight difference between the packages. You may review the package dimensions from the datasheet.

diazmarin09_0-1686334645315.png

 

I hope this information helps.

Regards,

David

在原帖中查看解决方案

2 回复数
607 次查看
DanKSI
Contributor III

That is the exact info I was looking for.

Thanks,

Dan K.

0 项奖励
618 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dan,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the SGTL5000XNAA3 device is obsolete.

In this case, you may use the SGTL5000XNBA3 device as a direct replacement.

Please be aware that there is a slight difference between the packages. You may review the package dimensions from the datasheet.

diazmarin09_0-1686334645315.png

 

I hope this information helps.

Regards,

David