Is NTB0102 suitable for uart aplication?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is NTB0102 suitable for uart aplication?

ソリューションへジャンプ
1,983件の閲覧回数
ugurozkan52
Contributor II

Hello Dear,

I want to use NTB0102 as Uart Level shifter.

Is NTB0102 suitable for uart aplication?

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,979件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ugur,

Bidirectional voltage-level translators with automatic direction sensing as the NTB0102 are not recommended for unidirectional interfaces as the UART is. 

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,980件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ugur,

Bidirectional voltage-level translators with automatic direction sensing as the NTB0102 are not recommended for unidirectional interfaces as the UART is. 

Best regards,

Tomas

0 件の賞賛
返信
1,976件の閲覧回数
ugurozkan52
Contributor II
Thanks for reply.
0 件の賞賛
返信