Is NFC PN553 IC supports ISO/IEC 18092 for android Pie?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is NFC PN553 IC supports ISO/IEC 18092 for android Pie?

2,075 Views
niteshagrawal
Contributor I

Hi All,

I am using NFC PN553 IC with QCOM processor APQ8053 + Android Pie.

Is this IC supports ISO/IEC 18092?

If yes, do i need to add/change anything in Driver/Code?

Labels (6)
0 Kudos
Reply
1 Reply

1,634 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Seems PN553 is not for public. I cannot find any document or information for it.

Please contact the local marketing or FAE to request this product support.

0 Kudos
Reply