Input_capture imx93evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input_capture imx93evk

1,537 Views
Rakesh_Kumar-Thakur
Contributor III

Hi NXP

I am working on input capture driver provided by MCUXpresso SDK version 2.16. But I ran this driver on target machine with 100Hz frequency, so input capture value is coming different values ​​at the same given frequency. Clock source frequency is 24MHz which is given by TMR, prescaler value is 1. I have also configured other TPM counters and channels and tested them but the result is same. How to solve it.

thanks & regards

Tags (1)
0 Kudos
Reply
2 Replies

1,513 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Rakesh_Kumar-Thakur!

Thank you for contacting NXP Support!


I tried the demo by my side and is working good.


How are you validating your input signal?


I am using a MCXN to generate the 100 HZ signal and the iMX93 is not giving me the exact number every time but are values very close.


If you want to be sure if the TMP is working good I recommend to test it with an external microcontroller sending to the iMX93 a counted pulses to get exactly the same result in every test.


Best Regards!

Chavira

0 Kudos
Reply

1,314 Views
Rakesh_Kumar-Thakur
Contributor III

Hi @Chavira 

Thanks for reply I was working on another model and now i am working on input capture module , i have attached my application code in comment . i am giving input signal through function generator 100 Hz , i am using imx93evk MCUXPreso SDK version 2.25 ,

value is coming different on same frequency i have attached also  screen short of code output.

Rakesh_KumarThakur_0-1733223928683.pngRakesh_KumarThakur_0-1733223928683.png

 

 

 

 

 

 

 

 

 

 

 

 
/*
* Copyright (c) 2015, Freescale Semiconductor, Inc.
* Copyright 2016-2021 NXP
* All rights reserved.
*
* SPDX-License-Identifier: BSD-3-Clause
*/

#include <stdio.h>
#include "fsl_debug_console.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_tpm.h"

#include "fsl_common.h"
/*******************************************************************************
* Definitions
******************************************************************************/
/* Define instance */
#define DEMO_TPM_BASEADDR TPM2

/* Interrupt to enable and flag to read; depends on the TPM channel used */
#define BOARD_TPM_INPUT_CAPTURE_CHANNEL kTPM_Chnl_0

/* Interrupt to enable and flag to read; depends on the TPM channel used */
#define TPM_CHANNEL_INTERRUPT_ENABLE kTPM_Chnl0InterruptEnable
#define TPM_CHANNEL_FLAG kTPM_Chnl0Flag

/* Interrupt number and interrupt handler for the TPM instance used */
#define TPM_INTERRUPT_NUMBER TPM2_IRQn
#define TPM_INPUT_CAPTURE_HANDLER TPM2_IRQHandler

/* Get source clock for TPM driver */
#define LPTPM_CLOCK_ROOT kCLOCK_Root_Tpm2
#define LPTPM_CLOCK_GATE kCLOCK_Tpm2
#define TPM_SOURCE_CLOCK CLOCK_GetIpFreq(LPTPM_CLOCK_ROOT)

/* Adjust this based on expected signal frequency */
#define EXPECTED_MAX_FREQUENCY 1000U /* 1 kHz */
#define EXPECTED_MIN_FREQUENCY 1U /* 1 Hz */

/*******************************************************************************
* Variables
******************************************************************************/
volatile bool tpmIsrFlag = false;
volatile uint32_t counterStart = 0;
volatile uint32_t counterEnd = 0;
volatile uint32_t capturedValue = 0;

/*******************************************************************************
* Code
******************************************************************************/
void TPM_INPUT_CAPTURE_HANDLER(void)
{
if (TPM_GetStatusFlags(DEMO_TPM_BASEADDR))
{
tpmIsrFlag = true;

/* Capture the value */
capturedValue = TPM_GetChannelValue(DEMO_TPM_BASEADDR, BOARD_TPM_INPUT_CAPTURE_CHANNEL);

/* Capture the end counter value when the interrupt occurs */
counterEnd = DEMO_TPM_BASEADDR->CNT;

/* Clear interrupt flag */
TPM_ClearStatusFlags(DEMO_TPM_BASEADDR, TPM_CHANNEL_FLAG);
}
SDK_ISR_EXIT_BARRIER;
}

/*!
* @brief Main function
*/
int main(void)
{
tpm_config_t tpmInfo;

/* Board pin, clock, debug console init */
const clock_root_config_t lptpmClkCfg = {
.clockOff = false,
.mux = 0, /* Select clock source, e.g., system clock */
.div = 1 /* Adjust divider to match expected signal frequency */
};

BOARD_InitBootPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();

CLOCK_SetRootClock(LPTPM_CLOCK_ROOT, &lptpmClkCfg);
CLOCK_EnableClock(LPTPM_CLOCK_GATE);

/* Print a note to terminal */
PRINTF("\r\nTPM Input Capture with Counter Example\r\n");
PRINTF("Provide an input signal with frequency between %u Hz and %u Hz\r\n", EXPECTED_MIN_FREQUENCY, EXPECTED_MAX_FREQUENCY);
PRINTF("Waiting for input signal...\r\n");

TPM_GetDefaultConfig(&tpmInfo);
/* Initialize TPM module */
TPM_Init(DEMO_TPM_BASEADDR, &tpmInfo);

/* Setup input capture on a TPM channel */
TPM_SetupInputCapture(DEMO_TPM_BASEADDR, BOARD_TPM_INPUT_CAPTURE_CHANNEL, kTPM_RisingEdge);

/* Set the timer to be in free-running mode */
TPM_SetTimerPeriod(DEMO_TPM_BASEADDR, TPM_MAX_COUNTER_VALUE(DEMO_TPM_BASEADDR));

/* Enable channel interrupt when the edge is detected */
TPM_EnableInterrupts(DEMO_TPM_BASEADDR, TPM_CHANNEL_INTERRUPT_ENABLE);

/* Enable at the NVIC */
EnableIRQ(TPM_INTERRUPT_NUMBER);

TPM_StartTimer(DEMO_TPM_BASEADDR, kTPM_SystemClock);

/* Reset the counter */
DEMO_TPM_BASEADDR->CNT = 0;
counterStart = 0;

while (tpmIsrFlag != true)
{
/* Wait for the interrupt to occur */
}

/* Validate clock frequency */
uint32_t clockFrequency = TPM_SOURCE_CLOCK;
if (clockFrequency == 0)
{
PRINTF("\r\nError: Clock frequency is 0. Check the clock configuration.\r\n");
while (1)
;
}

/* Calculate elapsed time using counter values */
if (counterEnd >= counterStart)
{
uint32_t elapsedCounts = counterEnd - counterStart;
float elapsedTime = (float)elapsedCounts / (float)clockFrequency;

/* Validate and calculate frequency */
uint32_t signalFrequency = (capturedValue != 0) ? (clockFrequency / capturedValue) : 0;

/* Print results */
PRINTF("\r\nCounter Start Value: %u\r\n", counterStart);
PRINTF("Counter End Value: %u\r\n", counterEnd);
PRINTF("Elapsed Counts: %u\r\n", elapsedCounts);
PRINTF("TPM Source Clock Frequency: %u Hz\r\n", clockFrequency);
PRINTF("Elapsed Time: %.6f seconds\r\n", elapsedTime);
PRINTF("Estimated Signal Frequency: %u Hz\r\n", signalFrequency);
}
else
{
PRINTF("\r\nError: Counter end value is less than counter start value.\r\n");
}

while (1)
{
}
}


0 Kudos
Reply