Hello,
I intend to use the PCA9956B for color control of RGB LEDs. I see that the LEDOUT[5:0] registers can be used to group certain LEDs together by assigning LDRx = 0x11. That allows the GRPPWM register to control the PWM of that selected group of LEDs. However, since there is only 1 GRPPWM register, how can 2 or more different groups be created and independently controlled?
Specifically these groups:
1. Red Group
2. Green Group
3. Blue Group
That way the entire color set can be adjusted independently of each other. e.g. Raise all Red to 80% PWM and lower all Blue to 40% PWM. How can this be achieved using the PCA9956B driver.
Thank you