Increasing the distance communication range for PN 532 modules in P2P mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Increasing the distance communication range for PN 532 modules in P2P mode

668 Views
toshaxar
Contributor I

Hello! I've heard that you can increase the tag reading distance by increasing the antenna size. Could you provide a link to the methods with a description of this method. I also heard about the possibility of increasing the distance to 1.5 meters using special technology. Could you also provide links to materials with which I could solve such a problem to implement two-way transmission of information to and from the selected module to the same one at least at a distance of 1 meter (in P2P mode)?

0 Kudos
Reply
0 Replies