Image available for Grapeboard like Raspbian ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image available for Grapeboard like Raspbian ?

1,335 Views
wilbolinux
Contributor I

Hello everybody,

I'm experimenting on the grapeboard,
trying to build a working image.


Is there a way to download finished Linux images?
...and boot it from the SDCARD ?

That would be great !

Like Raspberrry with Rasbian :smileyhappy:

Thanks for your info!

Wilfried.

Labels (1)
0 Kudos
Reply
1 Reply

1,259 Views
Pavel
NXP Employee
NXP Employee

The LS1012a supports booting only from QSPI NOR Flash. See the Section 24.1 of the LS1012a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1012ARM

 

See the Chapter 4.1.1 of the LSDK 18.12 documentation about LSDK using for the FRWY-LS1012A board:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.12.pdf

 

See also the Section 4.1.1.4 about deploying LSDK images on the board.

 

The Section 8.6.3 in the ARMv8_Targeting_Manual.pdf file contains information about program U-Boot in flash device using Flash Programmer.

This file is available in CW4NET folder.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply