IMX93EVK indivual image flash steps

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93EVK indivual image flash steps

402 Views
ranga_yn
Contributor III

Hello NXP,

wanted to use the complete 32GB sd card boot for the IMX93EVK board. Could you please let me know the steps to flash the individual built images -on the SD card . with current single image flash its not displaying complete storage capcity.

 

thanks. R

0 Kudos
Reply
2 Replies

383 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi, 

You can refer to the section <Booting Linux OS> in IMX_LINUX_USERS_GUIDE.pdf 

 

Regards

Harvey

 

0 Kudos
Reply

370 Views
ranga_yn
Contributor III

Hello NXP team,

Thanks for the input. I want to use the complete SD card of 32 GB. So as it has less input of IMX93EVK.

I have below queries - how many partitions i have to make , And as i need to load boot, dtb and rootfs on SD , could you share me steps that would help other with IMX93EVK users.

 

regards,

r

0 Kudos
Reply