IMX8MP: 5.15 Linux kernel with 5.4 U-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP: 5.15 Linux kernel with 5.4 U-boot

1,365 Views
mahesh_hns
Contributor II

Hi,

 I have a imx8mp based board running 5.4 linux (and uboot too). I am in the process of migrating it to 5.15.71 linux. Does the 5.15.71 linux work with 5.4 uboot? (I am yet to migrate to 5.4 uboot). Any requirement of the uboot version being the same as the linux version between 5.4 and 5.15 ?

When I boot up the 5.15 linux, the linux kernel hangs with "Starting Kernel..." and I do not see anything further. I used imx_v8_defconfig as the config file.

Any pointers?

0 Kudos
Reply
1 Reply

1,344 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

They use different u-boot, please see the pictures below:

josephlinares_0-1711670805511.png

i.MX Linux Release Notes, Rev. L5.4.3_1.0.0, 03/2020

josephlinares_1-1711670866350.png

i.MX Linux Release Notes, Rev. LF5.15.71_2.2.0, 2 March 2023

Regards

0 Kudos
Reply