IMX8 enable HDCP function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8 enable HDCP function

2,011件の閲覧回数
ximenbingmeng
Contributor IV
At present, we are using the IMX8MQ chip. From the reference manual, we can see that the HDCP2.2 function of the IMX8 chip is configured with the HDCP enabled configuration register,

How can I obtain the HDCP keys for IMX8? And do you need encrypted videos?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,468件の閲覧回数
vishwa2000
Contributor I

We are using IMX8MQ board and want to enable the HDCP functionality on Android 14. We want make use of this support for WFD sink of the Miracast implementation. Is there any HDCP specific procedure that needs to be followed in getting it enabled on the board (in the form of h/w config or library etc.)

Is the HDCP enablement available for both Android and Linux variants for iMX8M series boards?

0 件の賞賛
返信

1,982件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

1.NXP does not support customer programming of HDCP keys for IMX8MQ.  

2.For NXP programmed HDCP keys, the customer is first confirmed as an “HDCP adopter”.  Once confirmed, a special part number will be configured for them.  This allows NXP to track which customers receive a particular HDCP key.  NXP uses their own keys to program the devices. 

You need create a SFDC ticket for this issue.

0 件の賞賛
返信