IMX27 PDK - blew up the program!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX27 PDK - blew up the program!

1,565件の閲覧回数
ckuecker
Contributor II

Hello,

 

I really did it now. While poking around in the demo kit, I managed to run linuxrc. I hit control-C as soon as I realized I had done something naughty, but the damage was done.

 

On boot, the terminal now appears to be attempting to operate in a non-printable foriegn language.

 

I fervently hope i can recover by reflashing the unit - but, once bitten, twice shy - where is the image I should flash?

 

Chuck Kuecker

0 件の賞賛
返信
1 返信

1,057件の閲覧回数
ckuecker
Contributor II

Attempting to erase the NAND flash via the ATK tool did not succeed, but it cleared the problem, mostly. THere are warnings about 'stale lock file' and the file system has issues now, but it's running again.

 

Now, the issue is: why do I get erase failures? I tried to reflash RedBoot according to the IMX27 PDK Linux Demo Readme, and it fails, too.

 

Anyone have any idea which way I should go next?

0 件の賞賛
返信