I need more P/E cycles... Does MRAM have a limited number of P/E cycles?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need more P/E cycles... Does MRAM have a limited number of P/E cycles?

2,213 Views
mikehockstein
Contributor I
Hello everyone,
 
I have an HCS12 microprocessor with EEPROM that only has 10,000 P/E cycles.  I need a lot more than this (hoping for 100,000).  MRAM seems promising but its hard to find the information i'm looking for. Like does it have a limited number of P/E cycles and if so, how many for the ones at freescale?
 
Also, if anyone could reccomend a good microprocessor with nonvolatile memory with more than 10,000 P/E cycles that would be GREAT too.  Thank you very much everybody.
Tags (2)
0 Kudos
Reply
1 Reply

1,259 Views
genuap
NXP Employee
NXP Employee
MRAM has an unlimited number of program/erase cycles. Also, it offers much faster writes than conventional NVRAM. I've seen demo's where they prgram and erase 1 billion cycles at a time. It takes about 30sec.

Here's more on MRAM:
http://www.freescale.com/webapp/sps/site/overview.jsp?code=TM_MRAM&fsrch=1

 ... Paul

0 Kudos
Reply