How to config and run 802.1AS(gptp) on the SJA1105 Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to config and run 802.1AS(gptp) on the SJA1105 Board

1,053 次查看
xinting_gu
Contributor II

I bought a SJA1105 Application Board to verify AVB strteam between SJA1105 and PC(Ubuntu OS)so on.

I had tried to set clock synchronization parameters SW MASTER on PC(run gptp on master mode),

and made a new configuration file
(refer: SJA1105\example_configs\create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000_AVB.bat)

and run test.bat to install the newconfig.hex.

But I could not running gptp on the SJA1105, I try log network capture by Wireshark.

I don,t get any  protocals data of SJA1105.

Please tell me if something wrong or missing. How to config SJA1105 as a Switch run gptp. 

Now I can't  register Docstore anymore. It says "

The registration of new accounts is current not possible."

How can I download  the "sw427402 - Drivers (0.2)". to me?

 

Best Regards.

标记 (1)
0 回复数