High input current on PCA9698 P-ports

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

High input current on PCA9698 P-ports

822 Views
manuelcaracuel
Contributor II

I am using the PCA9698 expander and I would like to have all GPIO P-ports activated, but I have low power. So, output signals will have a low current, around 8mA. This signals are going to be used to interface with other PCA9698 expander in the future, with its P-ports configured as inputs. So I want to know how much current flows into each P-port  in case of High signal and Low signal. They are the parameters Iih and Iil.

Thanks

0 Kudos
Reply
1 Reply

759 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

If configure as input port,we can only have the leakage current spec+/-1uA.

Thanks!

BR

0 Kudos
Reply