High input current on PCA9698 P-ports

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

High input current on PCA9698 P-ports

823 次查看
manuelcaracuel
Contributor II

I am using the PCA9698 expander and I would like to have all GPIO P-ports activated, but I have low power. So, output signals will have a low current, around 8mA. This signals are going to be used to interface with other PCA9698 expander in the future, with its P-ports configured as inputs. So I want to know how much current flows into each P-port  in case of High signal and Low signal. They are the parameters Iih and Iil.

Thanks

标记 (4)
0 项奖励
回复
1 回复

760 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

If configure as input port,we can only have the leakage current spec+/-1uA.

Thanks!

BR

0 项奖励
回复