Help retrieving password from eeprom

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help retrieving password from eeprom

3,595件の閲覧回数
scottshaffer
Contributor I
Hello, I have a karaoke machine what I have lost the bios password for and the machine is now locked and unable to use. I have received some help from the original owner in Japan and they have suggested to try to read the eeprom to retrieve the code. Is there a way I can unlock this eeprom chip and reset the chip to reprogram the password or retrieve the password from the chip? Is there a way to find the original *.bin file?
 
Thank you for your help? 
 
chip: PCF8593
Type:Clock/Calendar
0 件の賞賛
返信
1 返信

3,560件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Scott,

I have checked the PCF8593 datasheet and this RTC doesn't contain EEPROM. It contains registers, which if no alarm function is used, they can be used as RAM memory. You can access all registers in the PCF8593 by I2C interface.

JozefKozon_0-1643887804103.png

Please first check the alarm enable bit in Control and Status register, address 00h.

JozefKozon_1-1643887910145.png

If its 0, then the memory locations 08h to 0Fh are free RAM space and you can read what is in there through the I2C interface.

With Best Regards,

Jozef

0 件の賞賛
返信