Help for coding an equation on DSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Help for coding an equation on DSP

跳至解决方案
4,704 次查看
mr_max
Contributor IV

Hello ! I'm new here.

 

I try to write this equation for my DSP : Y(n) = 1/2 (X(n) + X(n-1)) . After assembling and lunch the code into the processor, there is no signal at the output of my DAC.

 

Below a part of the source code :

 

Code language : Assembler

Microprocessor : DSP 56374

 

 

with :

Y(n) : Output signal (TxBuffBase)

1/2 : Coefb0

X(n) : actual sample (Xn)

 

 

...

  move  #$0,b  ; Init X(n-1) for the first loop

AudioLoop

 

  jclr  #RightRx,x:LRFlag,*

  bclr  #RightRx,x:LRFlag

  move    x:RxBuffBase,a          ; <- ADC left input

; move    x:RxBuffBase+2,b        ; <- ADC right input  (not use for the moment ...)

 

  move  a,x:(r1)                    ;saving Xn for the next loop

  move  r1,x:Xn

  move  #coefb0,r0                  ; coefb0 declare as constant

  move  x:(r0),x1 

  add  b,a                          ; a=X(n)+X(n-1)

  move a,x0

  mpy  x0,x1,a                      ; a=1/2((X(n)+X(n-1))

  move  x:(Xn),b                    ; register b become X(n-1)

 

  move    a,x:TxBuffBase          ; -> DAC left output

; move    b,x:TxBuffBase+1        ; -> DAC right output (note use)

  jmp  AudioLoop

...

 

So what wrong with my code ? Does someone can help me pleas ?

 

note 1 : I'm a beginner.

note  2 : The complete source code is in the attachment.

 

 

 

Original Attachment has been moved to: LPFn1_cs.asm.zip

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
4,195 次查看
rocco
Senior Contributor II

Hi Maxime,

I can see that your program has two components: the I/O and the math. I did not analyze your code to determine where your problem is, as I thought you needed to rewrite the math portion. As far as the I/O portion, I can address that later.

I can see that you are trying to implement an "exponential averager" with a coefficient of a=.5

Here is some code that I have for an exponential averager:

;

; Use the TachVoltage from the ESAI and filter it into x:TachoVelocity.

; We use the exponential-averager formula:  Y(new) = a*X + (1-a)*Y(old)

; Where:  X is the new sample, x:ESAI_TachVoltage

;         Y(old) is the previous average, x:TachoVelocity

; and     Y(new) is the new average.

;

TachFilter_a:    equ    .5          ;'a' modified for Maxime to .5

;

    move    x:ESAI_TachVoltage,X0   ;get tacho voltage read from the ESAI DAC

    move    x:TachoVelocity,Y0      ;get the previous value of the velocity

    mpy     #TachFilter_a,X0,A      ; A =  (a)  * X

    mac     #1-TachFilter_a,Y0,A    ;   + (1-a) * Y(old)

    nop                             ;pipeline stall

    move    A,x:TachoVelocity       ;save filtered tacho voltage as motor velocity

;

A little explanation:

The actual averaging is done in only two instructions: a 'mpy' and a 'mac'.

Where you need to add two values, you can often use the "multiply-and-accumulate" instruction instead of an add. Much of the power of DSPs come from the 'mac' instruction, as many algorithms are based on adding successive products together.

Notice that in my above code, you can change the time-constant of the filter by changing the "TachFilter_a:  equ .5" line. The smaller 'a' is, the more filtering you have. Since the sum of 'a' and '1-a' is 1, the filter has unity gain.

You should only use the address registers R0-R7, N0-N7 and M0-M7 when working with addresses. Remember that the ALU and the AGU are two independent computational units, with very different purposes.

The I/O is an independent issue.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,196 次查看
rocco
Senior Contributor II

Hi Maxime,

I can see that your program has two components: the I/O and the math. I did not analyze your code to determine where your problem is, as I thought you needed to rewrite the math portion. As far as the I/O portion, I can address that later.

I can see that you are trying to implement an "exponential averager" with a coefficient of a=.5

Here is some code that I have for an exponential averager:

;

; Use the TachVoltage from the ESAI and filter it into x:TachoVelocity.

; We use the exponential-averager formula:  Y(new) = a*X + (1-a)*Y(old)

; Where:  X is the new sample, x:ESAI_TachVoltage

;         Y(old) is the previous average, x:TachoVelocity

; and     Y(new) is the new average.

;

TachFilter_a:    equ    .5          ;'a' modified for Maxime to .5

;

    move    x:ESAI_TachVoltage,X0   ;get tacho voltage read from the ESAI DAC

    move    x:TachoVelocity,Y0      ;get the previous value of the velocity

    mpy     #TachFilter_a,X0,A      ; A =  (a)  * X

    mac     #1-TachFilter_a,Y0,A    ;   + (1-a) * Y(old)

    nop                             ;pipeline stall

    move    A,x:TachoVelocity       ;save filtered tacho voltage as motor velocity

;

A little explanation:

The actual averaging is done in only two instructions: a 'mpy' and a 'mac'.

Where you need to add two values, you can often use the "multiply-and-accumulate" instruction instead of an add. Much of the power of DSPs come from the 'mac' instruction, as many algorithms are based on adding successive products together.

Notice that in my above code, you can change the time-constant of the filter by changing the "TachFilter_a:  equ .5" line. The smaller 'a' is, the more filtering you have. Since the sum of 'a' and '1-a' is 1, the filter has unity gain.

You should only use the address registers R0-R7, N0-N7 and M0-M7 when working with addresses. Remember that the ALU and the AGU are two independent computational units, with very different purposes.

The I/O is an independent issue.

0 项奖励
回复
4,195 次查看
mr_max
Contributor IV

Great ! It's work. I've made a test by sweeping a sinus wave and the output signal has been filtered. It isn't the best filter I've seen but it's a good start for me ! By the way, your equation is not exactly same of mine because X(n-1) isn't the previous average (like Y(old))  but the previous sample from the ADC. But thank you anyway. I understand a little more now what is the purpose of the MAC operation.

I've a question : Can I use MAC operation one after the other ?

For example if I want resolve Y(n) = b0.X(n) + b1.X(n-1) +b2.X(n-2)

The code will be :

coefb0:     equ     0.5

coefb1:     equ     0.4

coefb2:     equ     0.3


;This values of coefficients are for the exemple

move     x:RxBuffBase,X0           ;Take sample from ADC to X0 register

move     X0,x:Xn1                  ;X(n) -> X(n-1) ; I'm not sure that is a good data transfert. Is it ?

move     Xn1,x:Xn2                 ;X(n-1)-> X(n-2); Same thing, not sure ...

mpy      #coefb0,x0,a              ;a=b0*X(n)

mac      #coefb1,Xn1,a             ; + b1*X(n-1)

mac      #coefb2,Xn2,a             ; + b2*X(n-2)

nop                                ; Why we should do a non-operation here ?? What is a Pipeline Stall ??

move     a,x:TxBuffBase            ; TxBuffBase = intput DAC.


; Note : Xn, Xn1 and Xn2 have been declared into the X date memory.


I didn't test the code. I will do it later this day. Do you think is good like this ?

0 项奖励
回复
4,195 次查看
rocco
Senior Contributor II

Hi Maxime,

Your right, I misread your code. It looked so much like the exponential-averager that my brain told me it was. In reality, it was a two-tap FIR filter. Now I understand why the coefficients were .5

Your last question first: What is a pipeline stall?

Typically, the DSP starts an new instruction every cycle, but the execution is pipelined, so it typically takes 7 cycles to complete. In effect, 7 instructions are at different stages of execution at any point in time. The actual multiply in the ALU takes 2 cycles, so the result cannot be read-out of the accumulator until one cycle after the multiply is executed. I use a NOP for that one cycle delay, but if the NOP is not there, the DSP is supposed to insert a "pipeline-stall" auto-magically. However, my assembler flags an error when it detects a pipeline-stall, so I need to explicitly delay that one cycle.

As for the MAC instruction:

I see that you are expanding your FIR filter to three taps, and you are heading in the correct direction. But if you should expand to, say, 100 taps, you can see how the code can get tedious.

The "repeat" instruction, coupled with the MAC instruction and the Address Generation Unit (AGU) allows you to build a FIR filter of any size with just a few instructions. Here is a sample:

;

; Set N to the number of taps you would like to have.

;

N:    equ    32      ;for a 32 tap FIR filter

;

; This code only needs to be executed once to initialize the AGU registers.

;

    move    #CoefficientTable,R0   ;FIR filter coefficient table in x-memory

    move    #SampleTable,R4        ;samples-table to be filtered in y-memory

    move    #N-1,M4                ;set modulus register for N taps

    move    M4,M0                  ;both modulus registers are the same

.

.

.

;

; This code gets executed for each new sample.

;

    movep  y:input,y:(R4)          ;put sample in table over oldest sample

    clr    A         x:(R0)+,X0  y:(R4)-,Y0  ;get 1st sample and coefficent

    rep    #N-1                    ;do 'mac' for all taps except the last tap

      mac  X0,Y0,A   x:(r0)+,X0  y:(r4)-,Y0  ;get next sample and coefficient

    macr   X0,Y0,A   (r4)+         ;mac final tap, round, inc sample-address

    movep  a,y:output              ;ship the filtered value to the outside

;


Notice that the address registers take care of themselves, wrapping around from end to beginning when they need to. Notice also that the 'mac' instruction inside the repeat-loop not only multiplies and adds, but also fetches the next sample and coefficient for the following iteration. That means 1 cycle per tap. In the DSP that I'm using, it means I can execute a tap in 5 nanoseconds, or a 100 tap FIR filter in half a microsecond.

4,195 次查看
mr_max
Contributor IV

Waw I'm realy impressed by the power of parallel operation. Thank you Mark for your knowledge. Your tips will be very helpful for my second grade bachelor ! :smileyhappy:

Two last question :

What do you mean by set modulus register for N taps ?

And why did you copy M4 into M0 registers ?

0 项奖励
回复
4,195 次查看
rocco
Senior Contributor II

Hi Maxime,

Two last question :

What do you mean by set modulus register for N taps ?

And why did you copy M4 into M0 registers ?

Well, thats the way modulo-addressing works - the modulus is handled in hardware, as determined by the respective Mn register. And of course the number of samples is equal to the number of coefficients, so both modulo registers need to be the same.

You may want to re-read the chapter on the Address Generation Unit. I had to read the DSP family-manual a couple of times before I understood how everything worked.

0 项奖励
回复