Has anyone attempted to build the Android Pie environment on Ubuntu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Has anyone attempted to build the Android Pie environment on Ubuntu?

1,167 次查看
joelamanna92
Contributor I

./scripts/gcc-version.sh: line 26: gcc: command not found
./scripts/gcc-version.sh: line 27: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
./scripts/gcc-version.sh: line 26: gcc: command not found
./scripts/gcc-version.sh: line 27: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
make: Leaving directory '/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx'
make: Entering directory '/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx'
make[1]: Entering directory '/home/thebeast/android_build/out/target/product/evk_8mq/obj/KERNEL_OBJ'
HOSTCC scripts/basic/fixdep
/bin/bash: gcc: command not found
make[3]: *** [scripts/Makefile.host:102: scripts/basic/fixdep] Error 127
make[2]: *** [/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx/Makefile:464: scripts_basic] Error 2
make[2]: *** Waiting for unfinished jobs....
GEN ./Makefile
make[1]: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/kernel.release'. Stop.
make[1]: Leaving directory '/home/thebeast/android_build/out/target/product/evk_8mq/obj/KERNEL_OBJ'
make: *** [Makefile:146: sub-make] Error 2
make: Leaving directory '/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx'
[ 0% 165/92660] target C++: libv8src <= external/v8/src/snapshot/deserializer.cc
[ 0% 166/92660] target C++: libv8src <= external/v8/src/snapshot/partial-serializer.cc
[ 0% 167/92660] target C++: libv8src <= external/v8/src/snapshot/serializer-common.cc
[ 0% 168/92660] target C++: libv8src <= external/v8/src/snapshot/snapshot-source-sink.cc
[ 0% 169/92660] target C++: libv8src <= external/v8/src/snapshot/serializer.cc
[ 0% 170/92660] target C++: libv8src <= external/v8/src/snapshot/startup-serializer.cc
[ 0% 171/92660] target C++: libv8src <= external/v8/src/snapshot/snapshot-common.cc
[ 0% 172/92660] target C++: libv8src <= external/v8/src/source-position-table.cc
[ 0% 173/92660] target C++: libv8src <= external/v8/src/source-position.cc
ninja: build stopped: subcommand failed.
13:28:54 ninja failed with: exit status 1

#### failed to build some targets (03:43 (mm:ss)) ####

thebeast@ubuntu:~/android_build$

0 项奖励
回复
1 回复

873 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Did you installed the required packages? not even the ones that we specify on the documentation. There are more packages that need to be installed to build the android image. Those packages are specified on the Android web page.

Establishing a Build Environment  |  Android Open Source Project 

Hope this information can help you.

Best regards,

Diego.

0 项奖励
回复