Has anyone attempted to build the Android Pie environment on Ubuntu?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has anyone attempted to build the Android Pie environment on Ubuntu?

1,064件の閲覧回数
joelamanna92
Contributor I

./scripts/gcc-version.sh: line 26: gcc: command not found
./scripts/gcc-version.sh: line 27: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
./scripts/gcc-version.sh: line 26: gcc: command not found
./scripts/gcc-version.sh: line 27: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
/bin/bash: gcc: command not found
make: Leaving directory '/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx'
make: Entering directory '/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx'
make[1]: Entering directory '/home/thebeast/android_build/out/target/product/evk_8mq/obj/KERNEL_OBJ'
HOSTCC scripts/basic/fixdep
/bin/bash: gcc: command not found
make[3]: *** [scripts/Makefile.host:102: scripts/basic/fixdep] Error 127
make[2]: *** [/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx/Makefile:464: scripts_basic] Error 2
make[2]: *** Waiting for unfinished jobs....
GEN ./Makefile
make[1]: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/kernel.release'. Stop.
make[1]: Leaving directory '/home/thebeast/android_build/out/target/product/evk_8mq/obj/KERNEL_OBJ'
make: *** [Makefile:146: sub-make] Error 2
make: Leaving directory '/home/thebeast/android_build/vendor/nxp-opensource/kernel_imx'
[ 0% 165/92660] target C++: libv8src <= external/v8/src/snapshot/deserializer.cc
[ 0% 166/92660] target C++: libv8src <= external/v8/src/snapshot/partial-serializer.cc
[ 0% 167/92660] target C++: libv8src <= external/v8/src/snapshot/serializer-common.cc
[ 0% 168/92660] target C++: libv8src <= external/v8/src/snapshot/snapshot-source-sink.cc
[ 0% 169/92660] target C++: libv8src <= external/v8/src/snapshot/serializer.cc
[ 0% 170/92660] target C++: libv8src <= external/v8/src/snapshot/startup-serializer.cc
[ 0% 171/92660] target C++: libv8src <= external/v8/src/snapshot/snapshot-common.cc
[ 0% 172/92660] target C++: libv8src <= external/v8/src/source-position-table.cc
[ 0% 173/92660] target C++: libv8src <= external/v8/src/source-position.cc
ninja: build stopped: subcommand failed.
13:28:54 ninja failed with: exit status 1

#### failed to build some targets (03:43 (mm:ss)) ####

thebeast@ubuntu:~/android_build$

0 件の賞賛
返信
1 返信

770件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Did you installed the required packages? not even the ones that we specify on the documentation. There are more packages that need to be installed to build the android image. Those packages are specified on the Android web page.

Establishing a Build Environment  |  Android Open Source Project 

Hope this information can help you.

Best regards,

Diego.

0 件の賞賛
返信